MS5803-14BA Pressure Sensor Hookup Guide

≡ Pages
Contributors: CaseyTheRobot

Introduction

The MS5803-14BA is a pressure sensor with an I2C ("Wire") and SPI interface.

SparkFun Pressure Sensor Breakout - MS5803-14BA

SEN-12909
$80.50

Pressure sensors measure the absolute pressure of the fluid around them. This includes air, water, and anything else that acts like a viscous fluid. Depending on how you interpret the data, you can determine altitude, water depth, or any other tasks that require an accurate pressure reading.

Covered in This Tutorial

We will show you how to connect this sensor to an Arduino microcontroller and use the included software library to get measurements out of the sensor. We'll also show you how to interpret the readings showing changes in altitude and water depth.

Suggested Reading

This part is easy to use. But before you start, we recommend the following background knowledge:

How to Solder: Through-Hole Soldering

This tutorial covers everything you need to know about through-hole soldering.

Working with Wire

How to strip, crimp, and work with wire.

What is an Arduino?

What is this 'Arduino' thing anyway? This tutorials dives into what an Arduino is and along with Arduino projects and widgets.

Logic Levels

Learn the difference between 3.3V and 5V devices and logic levels.

I2C

An introduction to I2C, one of the main embedded communications protocols in use today.