MP3 Player Shield Hookup

This Tutorial is Retired!

This tutorial covers concepts or technologies that are no longer current. It's still here for you to read and enjoy, but may not be as useful as our newest tutorials.

View the updated tutorial: MP3 Player Shield Hookup Guide V15

≡ Pages
Contributors: jimblom

Hardware Overview

The centerpiece of the MP3 Player Shield is a VS1053B Audio Codec IC. The VS1053B is a multitalented little chip. On top of MP3's, it can also decode Ogg Vorbis, AAC, WMA, and MIDI. (It's also capable of encoding audio, although that's outside the scope of the MP3 Shield.)

Supporting the VS1053 is a µSD card socket, which you can use to store MP3 files on. Using the Arduino SD library, it's simple to read music files off an SD card, and stream them to the VS1053B. There's additional circuitry on-board to level shift signals down to the 3.3V maximum allowable by SD cards.

Here's a quick visual overview of the important connectors and other components on the MP3 Player Shield:

Annotated Shield Image

In the image above, the blue labels are pins used by the VS1053 MP3 Codec IC, the red labels are used for communication with the µSD card, and the purple-labeled pins are used by both components (yay SPI!).

Which Pins are Being Used?

The MP3 Player Shield requires exclusive use of a handful of pins. These pins can't be used to interface with other devices:

  • D2 is connected to the data request output of the VS1053B. This pin is an interrupt, which tells the Arduino that the IC needs more music data.
  • D6 is connected to the chip select input of the VS1053B. This active-low pin tells the chip when data is being sent to it.
  • D7 is connected to the data chip select input of the VS1053B, which tells the chip when music data is being sent.
  • D8 is connected to the reset input of the VS1053B.
  • D9 is connected to the chip select input of the µSD card.

The Arduino's three SPI data and clock pins -- D11, D12, and D13 -- can be used to interface to other SPI components. They can't, however, be used for any purpose other than SPI.

Which Pins are Free?

Whew! The shield does use up quite a few pins, but here are the pins still available to connect to other components.

  • The hardware UART pins -- RX and TX -- on pins 0 and 1
  • D5 and D10 (PWM pins!)
  • All analog pins (A0 through A5).

Optional Pin Jumpers

Two pins we haven't mentioned yet are D3 and D4, which are connected to the VS1053B's MIDI-In and GPIO1 pins respectively. Use of these pins is optional. They're not required for most MP3-playing functions, including the examples we'll show in this tutorial.

Jumper location

To disable either of those pins, a jumper next to their label can be cut using a hobby knife.

Getting Audio Out

There are two options for driving audio out of the MP3 Player Shield. The easiest, most plug-and-play option is to stick some headphones into the on-board 3.5mm stereo audio jack. Active (powered) speakers could also be plugged into this jack, but the VS1053B alone doesn't have enough power on its own to drive low-impedance, passive speakers.

Audio output location

The right and left channels, as well as the audio ground are also broken out to a 0.1" header next to the headphone jack. You can use these pins to connect up to a speaker or amplifier input.

Line Out Warning

If you're going to connect the speaker output to power amplifiers or circuits, make sure you read through VLSI's Connecting analog outputs application note.

The pin labeled '-' next to 'R' and 'L' is connected to the 'GBUF' pin on the VS1053B. This pin isn't ground, and shouldn't be connected to ground! It's biased internally in the VS1053B to 1.25V. If GBUF is connected to a line-in input on a PC, for example, it could be connected on the PC side to ground and form a ground loop.

How to make a ground loop

A dangerous (to the VS1053B) current loop can be created if GBUF is connected to an amplifiers ground. (From the VS10XX Analog Output App Note.)

Don't do that! The VLSI app note has some recommended circuits (see sections 3.1 and 3.2) to help avoid this kind of problem.