MicroMod Main Board Hookup Guide V2
Contributors:
bboyho,
Elias The Sparkiest
Resources and Going Further
Now that you've successfully got your MicroMod Main Board with a Processor Board, it's time to incorporate it into your own project! For more information, check out the resources below:
- MicroMod Main Board - Single V2.1
- MicroMod Main Board - Double V2.2
Looking for more inspiration? Check out these other tutorials related to MicroMod.
MicroMod RP2040 Processor Board Hookup Guide
This tutorial covers the basic functionality of the MicroMod RP2040 Processor Board and highlights the features of the dual-core ARM Cortex-M0+ processors development board. Get started with the first microcontroller from the Raspberry Pi Foundation!
MicroMod WiFi Function Board - ESP32 Hookup Guide
The MicroMod ESP32 Function Board adds additional wireless options to MicroMod Processor Boards that do not have that capability. This special function board acts as a coprocessor that takes advantage of Espressif's ESP32 WROOM to add WiFi and Bluetooth® to your applications.
MicroMod mikroBUS™ Carrier Board Hookup Guide
This carrier board takes advantage of the MicroMod, Qwiic, and the mikroBUS™ ecosystems and allows users to take advantage of the growing number of 7 MicroMod processor boards, 83 Qwiic (add-on) boards, and +1100 drop-in Click boards™, which equates to +51M different board combinations. Click to learn more.