LilyPad Temperature Sensor Hookup Guide

≡ Pages
Contributors: Gella

Attaching to a LilyPad Arduino

The LilyPad Temperature Sensor has three sew tabs - Power (+), Ground (-), and Signal (S). The signal tab will be connected to an analog tab (marked with an 'A') on a LilyPad Arduino.

LilyPad Arduino USB

To follow along with the code examples in this tutorial, connect the temperature sensor to a LilyPad Arduino as shown below. Use alligator clips to temporarily connect Signal to A3 on a LilyPad Arduino, (-) to (-) on the LilyPad, and the (+) to (A5). When you are finished prototyping, replace the alligator clips with conductive thread traces for permanent installation in your project.

Attaching Sensor to a LilyPad USB

LilyPad ProtoSnap Plus

Attaching Sensor to a LilyPad ProtoSnap Plus

After clipping the sensor to A9, move the slide switch to the OFF position to keep the switch from interfering with your input signal.

Turn Switch OFF for A9

Other LilyPad Connection Notes:

  • If using the ProtoSnap - LilyPad Development Simple - attach to the metal tab at the top right of the board, this connects to A3. You can also set pin A5 to HIGH in your code to use it as an additional power tab, as the LilyPad Simple's tab is hard to access in the ProtoSnap format.
  • If using the the pre-wired temperature sensor on the ProtoSnap - LilyPad Development Board, it is attached to pin A1.