Let It Glow Holiday Cards

≡ Pages
Contributors: Gella

Step 1: Print Templates

Right-click the images below and choose “Save Link As” to download the templates to your computer. Each file has two (or three) pages which includes all pop up pieces and the circuit template.

Print your templates out on cardstock. If needed, adjust your printer's margins or choose 'Fit to Page' in the print settings. The card template is slightly smaller than the paper, make sure to cut along the black border for the final card size.

Set the pop up pages aside for now. We'll build our circuit first and then assemble the pop up once the electronics are all installed.

alt text)

Gingerbread House Template - 3 pages

Print page 2 (pop up pieces) on brown cardstock for a great gingerbread house base, or print all on a light colored cardstock and color in when you are finished. Can also be used to create a winter cottage pop up.

alt text

Christmas Tree Template - 2 pages

Looks great if printed on green cardstock, or use light colored cardstock and decorate after assembling.

alt text

Window Template - 2 pages

Use stickers or paper cut outs on vellum to create a festive silhouette scene in the window frame.