IOTA (ARTIC R2) Satellite Communication Module Hookup Guide

≡ Pages
Contributors: PaulZC

Castellated Pads

The IOTA has 24 castellated pads. It can be reflowed or hand-soldered onto a PCB depending on your needs.

You will find an Eagle symbol and footprint for IOTA in the SparkFun Eagle Libraries RF Library.

The photo below shows the bottom of IOTA. Pad 1 is top right.

Pictured are the I O T A castellated pads

The table below describes the function of each of the IOTA's castellated pads. Looking at IOTA from the top, pad 1 is top left. Pad numbering is counter-clockwise.

Pictured is pad 1

Pad No.NameFunctionDescription
1G8INPUTPull up to 3.3V to set the RFPA0133 transmit power to maximum. The transmit power will be reduced by _approximately_ 5dB if this pin is pulled low or left open.
23.0V OutOUTPUTThis pad allows measurement of the module's internal 3.0V rail.
3BOOTINPUTConnected to the ARTIC BOOT pin. Pulled up to 3.3V via a 100k resistor. When high, the ARTIC boots from the external flash memory. Pull low if the ARTIC firmware will be downloaded by the MCU via SPI.
4INT1OUTPUTConnected to the ARTIC INT1 pin. Will be pulled up to 3.3V by the ARTIC to indicate (e.g.) an RX_VALID_MESSAGE.
5INT2OUTPUTConnected to the ARTIC INT2 pin. Will be pulled up to 3.3V by the ARTIC to indicate (e.g.) an RX_BUFFER_OVERFLOW.
6RESETBINPUTConnected to the ARTIC reset pin. Pulled up to 3.3V via a 100k resistor. Pull low to reset the ARTIC.
7CSINPUTSPI interface Chip Select. 3.3V. Active low.
8SCLKINPUTSPI interface clock signal. Typically 1MHz. 3.3V. See the ARTIC R2 datasheet for the permitted clock speeds.
9COPIINPUTSPI interface: Controller Out Peripheral In. 3.3V.
10CIPOOUTPUTSPI interface: Controller In Peripheral Out. 3.3V.
111.8V OutOUTPUTThis pad allows measurement of the module's internal 1.8V rail.
12GNDPower ground / 0V.
13GNDPower ground / 0V.
14VININPUT3.3V power supply for the module. Voltage must be: 3.3V +/- 0.1V. Current limit: 500mA.
15PWR ENINPUTPulled low via a 10k resistor. Pull up to 3.3V to enable power for the ARTIC R2.
16FLASH_PWRINPUT3.3V power supply for the internal flash memory. Connect to Pin 17 (3.3V Out).
173.3V OutOUTPUTConnected to the module's internal 3.3V rail (switched) and provides power for the internal flash memory. Connect to Pin 16 (FLASH PWR).
18FLSH SCLKClock signal for the internal SST25VF020B 2-Mbit SPI Serial Flash. Used when programming the internal flash memory. Leave unconnected.
19FLSH SISerial Data In for internal SST25VF020B 2-Mbit SPI Serial Flash. Used when programming the internal flash memory. Leave unconnected.
20FLSH SOSerial Data Out for internal SST25VF020B 2-Mbit SPI Serial Flash. Used when programming the internal flash memory. Leave unconnected.
21FLSH CENChip Enable for internal SST25VF020B 2-Mbit SPI Serial Flash. Used when programming the internal flash memory. Leave unconnected.
22GNDPower ground / 0V.
23ANTENNARFAntenna connection (50 Ohm). Connected internally to the center pin of the u.FL connector.
24GNDPower ground / 0V.