Hookup Guide for the BlackBoard Artemis Nano

This Tutorial is Retired!

This tutorial was written for the SparkX version of this board. Please refer to the latest tutorial for up to date information.

View the updated tutorial: Hookup Guide for the SparkFun RedBoard Artemis Nano

≡ Pages
Contributors: Nate, Ell C

Hardware Overview

Power, GPIOs and GND Connections

The Nano breaks out 17 GPIO to PTH holes. Each GPIO is paired with a ground connection. We found the extra grounds immeasurably useful when wiring up projects; you'll often need a separate ground for each LED, button, or sensor. The Nano makes it that much easier to prototype an idea.

Pin Rails on the front and back of the Artemis Nano

Power is automatically selected between USB, LiPo, and Vin (Vin takes precedence). The VIN pin can handle up to 6V and will be regulated down to 3.3V using the AP2112 voltage regulator (600mA max output). The 3.3V pin can be used to power various 3.3V devices up to 600mA.

USB C and Serial Bootloading

We've designed the Nano with a reversible USB C connector and the CH340E USB to serial IC. This is an amazing IC that is small enough to fit under the USB C connector. The driver should automatically install on most operating systems. However, there is a wide range of operating systems out there. You may need to install drivers the first time you connect the chip to your computer's USB port or when there are operating system updates. For more information, check out our How to Install CH340 Drivers Tutorial. Also be sure to checkout our CH340 hookup guide for tips on using the CH340.

How to Install CH340 Drivers

August 6, 2019
How to install CH340 drivers (if you need them) on Windows, Mac OS X, and Linux.

SparkFun Serial Basic CH340C Hookup Guide

December 13, 2018
SparkFun Serial Basic Breakout takes advantage of USB-C and is an easy-to-use USB-to-Serial adapter based on the CH340C IC from WCH. With USB-C you can get up to three times the power delivery over the previous USB generation and has the convenient feature of being reversable.

SparkFun Artemis Nano with USB highlighted

The current USB C configuration is with two 5.1k Ohm resistors. This will allow up to 2 amps at 5 volts from your USB source. Nearly all modern computers and battery packs have short circuit protection but just be aware that the Nano does not have any short circuit protection.

Reset and Power Control

The Nano is a great device to embed in a project. But if it's embedded, it is often impossible to access the reset and power switches on a board. We've exposed the reset pin and an I/O pin. This is a perfect place to solder a big external power switch. The I/O pin controls the enable line on the 3.3V regulator. Pull this line low and the board will turn off. Release the I/O line and the board will run normally. The enable line is pulled high with a resistor so if you don't hookup anything the board will operate normally.

SparkFun Artemis reset and power switch

RTC and PDM Microphone

The Artemis has built in RTC capabilities if it is given a 32kHz source so we've added a 32kHz crystal to the Nano. Additionally, one of the main applications of the Artemis is voice recognition so we've added a MEMS digital PDM microphone to the board so that you can capture and analyze audio.

SparkFun Artemis Nano mic and RTC

LiPo Battery and Charging

The Nano has integrated LiPo power and charging. Any one of our LiPo batteries with work great with the Nano. The CHG LED will illuminate while the battery is charging via USB and will turn off when the battery is at peak voltage. Charge rate is set to 500mA. The general rule of thumb is charge no faster than 1C so the minimum recommended battery size is a 500mAh battery, but any of the larger batteries will work just fine.

LiPo Battery and Charging highlighted