Getting Started with the BrickPi

This Tutorial is Retired!

This tutorial covers concepts or technologies that are no longer current. It's still here for you to read and enjoy, but may not be as useful as our newest tutorials.

≡ Pages
Contributors: Shawn Hymel

BrickPi Assembly

You will need to build the hardware around the BrickPi in order to connect it to the Raspberry Pi and your building blocks.

Build the Case

1) Unpack the BrickPi hardware and remove the protective paper from the case.

BrickPi parts

2) Screw the two small standoffs into the holes in the bottom piece of acrylic.

BrickPi assembly

3) Screw a Raspberry Pi onto the two bottom standoffs.

Raspberry Pi in BrickPi case

4) Screw the four long standoffs into corner slots of the bottom piece of acrylic.

BrickPi assembly process

5) Attach the BrickPi to the Raspberry Pi by mating the BrickPi's header to the Raspberry Pi's GPIO header.

BrickPi mounted on Raspberry Pi

6) (Optional) Now is a good time to label the motor and sensor ports on the BrickPi. I recommend S1, S2, and so on for the sensor ports and MA, MB, and so on for the motor ports.

BrickPi with labels

7) Attach the top piece of acrylic to the four posts using the remaining screws.

Fully assembled BrickPi with Raspberry Pi

8) Insert the SD card.

SD Card in Raspberry Pi inside BrickPi case

Attaching the Building Blocks

Beams can be attached to the top and bottom pieces of acrylic in order to secure the BrickPi and Raspberry Pi to your building block creation.

Lego pegs in BrickPi case

Attach pegs to the holes in the acrylic

Lego beam on BrickPi case

Attach beams to the pegs

Any of the Mindstorms sensors can be attached to the ports labeled with an "S" followed by a number. You will need to remember the port number that you plugged your sensor into.

BrickPi Lego motor port locations

Sensor port locations (Image courtesy of dexterindustries.com)

Motors can be attached to the ports labeled with an "M" followed by a letter.

BrickPi Lego sensor port locations

Motor port locations (Image courtesy of dexterindustries.com)

For this example, connect a single touch sensor to S1 and a single servo motor to MA.

Sensor and motor connected to the BrickPi

Connect Peripherals

Similar to the setting up the Raspberry Pi tutorial, we need to connect a keyboard, mouse, and monitor. Plug a keyboard and mouse into the USB ports, and connect a monitor using an HDMI cable.

BrickPi and Raspberry Pi with connected peripherals