EL Wire Light-Up Dog Harness

≡ Pages
Contributors: jenfoxbot

Programming

Now it's time to program the electronics.

Connect EL Sequencer to computer via 5V FTDI BOB or cable.

Program the EL Sequencer using the Arduino platform; the EL Sequencer runs an ATmega 328p at 8 MHz and 3.3V.

Write a program to read in the analog value of the ambient light sensor, turn on the appropriate EL wire channels at a value that corresponds to low light, and turn off once the light sensor value is above the low light threshold.

Below is a sample Arduino sketch with a preset light threshold:

language:c
// EL Wire Dog Harness Program
// Turn EL wire on when ambient light is low.
// JenFoxBot
// Based on test sketch by Mike Grusin, SparkFun Electronics

void setup() {
  Serial.begin(9600);  
  // The EL channels are on pins 2 through 9
  // Initialize the pins as outputs
  pinMode(2, OUTPUT);  // channel A  
  pinMode(3, OUTPUT);  // channel B   
  pinMode(4, OUTPUT);  // channel C
  pinMode(5, OUTPUT);  // channel D    
  pinMode(6, OUTPUT);  // channel E
  pinMode(7, OUTPUT);  // channel F
  pinMode(8, OUTPUT);  // channel G
  pinMode(9, OUTPUT);  // channel H
  // We also have two status LEDs, pin 10 on the Escudo, 
  // and pin 13 on the Arduino itself
  pinMode(10, OUTPUT);     
  pinMode(13, OUTPUT); 
  pinMode(A2, INPUT);  
}

void loop() 
{
  int x,status;

  //If ambient lighting is too low, turn on EL wire
  if(analogRead(A2) < 50){
    digitalWrite(2, HIGH); //turn EL channel on
    delay(1000); //wait 1 second

    //Keep EL wire on until light sensor reading is greater than 50
    if(analogRead(A2) > 50){
      digitalWrite(2, LOW); //turn EL channel off
      delay(10);
    }

    Serial.println(analogRead(A2)); // Use this to check value of ambient light 

    digitalWrite(10, status);   // blink both status LEDs
    digitalWrite(13, status);
  }
}

Check that the EL wire turns on when the ambient light is low and turns off in bright light.