CAN-BUS Shield Hookup Guide

≡ Pages
Contributors: Toni_K, Member #399586

Hardware Overview

There are several features to be aware of on the CAN-Bus Shield.

Shield-Labeled

CAN-Bus Shield with features labeled.

1. DB9 Connector

The primary hardware feature on this shield is the DB9 connector. This allows you to interface to OBD-II ports with a DB9 to OBD-II cable.

2. GPS Connector

The GPS connector on-board is a 6-pin, JST SH compatible connector. The board is designed to interface with either the EM-506 GPS Receiver, or the GP-735 GPS Receiver. The GND jumper allows the user to modify the GPS connector for units that do not have a GND connection on pin 5 of the connector.

3. LCD Connector

The LCD footprint on the shield is compatible with a male 3-pin JST connector and can interface with any of our serial LCD screens. The connection is designed for 5V LCDs, so don't accidentally plug in a 3.3V option! The pin order is 5V, GND, and RX/D6 when looking at the shield straight on.

4. JoyStick

The joystick included on the shield provides a basic user interface for controlling screen displays or selecting CAN scan settings. The connector gives 5 basic user options:

  • Up
  • Down
  • Left
  • Right
  • Click selection

5. microSD Slot

This slot provides the user with the option of storing collected data onto a microSD card. Data collected can include user input on the joystick, CAN-Bus information collected, LCD outputs, or general I/O data.

6. Jumpers

There are six jumpers present on the CAN-Bus Shield.

  • 6a. SJ1 and SJ2 - These two jumpers allow the user to select between UART and Software Serial for the GPS unit to communicate with the Arduino.

  • 6b. SJ3 - This allows the user to separate pin 5 on the GPS connector from the GND line. This jumper comes closed by default.

  • 6c. SJ4, SJ5, and SJ6 - These three jumpers allow the user to select the DB9 pin configuration between OBD-II and CAN. The jumpers are defaulted to the OBD-II configuration that matches SparkFun's OBD-II to DB9 cable.

Note: Though the pin configuration is labeled as OBD-II, this is still a *CAN-specific* device. The jumpers are simply for configuring the shield to work with other OBD-II/CAN-Bus **cables** if necessary.

For reference, here are the configuration options showing which pins are selected on the DB9 connector for each setting.

Jumper Configurations for DB9 Pins
Bus LinesCAN PinsOBD-II PinsSolder Jumper
CAN-HPin 7Pin 3SJ4
CAN-LPin 2Pin 5SJ6
GNDPin 3Pin 2SJ5

7. CAN Pins

4 CAN lines are broken out to allow you direct access to the raw CAN data coming off of the DB9 connector. These pins are:

  • 5V
  • GND
  • CAN H (CAN HIGH)
  • CAN L (CAN LOW)

Again, this data is raw coming off of the CAN-Bus. It has not been filtered through the MCP2515 or the MCP2551 ICs.

Communication Methods

Because of all of the different hardware features on the shield, there are a couple different communication methods used.

  • SPI - The MCP2515 IC and the microSD slot both communicate with the Arduino via the SPI lines. The CAN Chip Select line is located on D10. The SD Chip Select line is connected to D9.

  • Analog In - The joystick is connected to pins A1-A5 on the Arduino. Each direction of the joystick has its own analog input.

  • Software Serial/UART - The LCD and GPS both communicate over serial lines with the Arduino. The LCD's RX line connects to D6. The GPS either connects via Software Serial to D4 and D5, or to the UART port on D0 and D1.