CAN-BUS Shield Hookup Guide

≡ Pages
Contributors: Toni_K, Member #399586

Hardware Hookup

Solder Connectors

To get your CAN-Bus shield hooked up, solder on the Arduino Stackable Headers.

Headers Inserted

You can use the RedBoard to hold the headers in place while soldering them to the shield.

Once those are soldered, consider how you want to connect your LCD screen. You can use either male or female headers with 0.1" spacing, or the JST connector. Solder your interface choice onto the shield at this time as well.

LCD

Make sure you solder the connector onto the top of the shield, so you can access it while the shield is inserted in the RedBoard.

Connect the Brain!

In our case, the brain will be the RedBoard. Insert your shield into the RedBoard. Take your time and go slowly to prevent bending the header pins.

Connect the Extras

We recommend plugging in the GPS unit, LCD screen, and microSD card now. If you don't plan to use any of these features, you can skip this step.

If you're planning on putting your CAN-Bus/RedBoard combination into an enclosure, you may want to consider using an extension cable for the GPS unit. Enclosures can block the satellites from view and lead to spotty GPS functionality, so placing the GPS unit outside of any enclosures should alleviate those issues.

Note: If you are not using the EM-506, verify the pinout of your GPS unit and make sure the GND jumper is in the proper configuration for your unit.

We also recommend connecting your LCD screen at this time. Your method of connecting the LCD screen will depend on what connector you soldered onto the shield previously. Looking the shield straight on, the connections are 5V, GND, and TX, if you are not using the JST connector.

Make sure you use a formatted microSD card. Once all the extras are connected, your circuit should look like the following:

GPS Inserted

Connect to your CAN-enabled device

This can be a simulator or a vehicle. Plug the DB9 connector into the shield, and plug the DLC connector into the device to which you plan on talking. If your shield+Arduino turns on now, that's ok. The vehicle/simulator can power the board over the cable.

Final Circuit

Once everything is inserted, your circuit should look similar to the following:

Connected to Simulator

In this case, we show the circuit connected to a CAN simulator. However, you could instead have your circuit connected to a DLC in a CAN-enabled vehicle.

Connected to Car

Here we see the circuit connected to Pete Dokter's VW.