Benchtop Power Board Kit Hookup Guide

≡ Pages
Contributors: Toni_K

Board Overview

The Benchtop Power Board Kit enables you to power up embedded electronics projects from a benchtop power supply. The kit breaks out the most commonly used voltages for physical computing projects to binding posts, including 3.3V, 5V, 12V and -12V.

Each power rail is spaced to fit banana jacks, and has a replaceable 5A fuse on it. It connects to a standard computer supply via an ATX connector. This board will require assembly before use.

SparkFun Benchtop Power Board Kit

KIT-12867
Retired

To complete this tutorial, you will need the following materials.

  • Benchtop Power Board Kit
  • Power Supply with an ATX connector
  • Standard soldering materials
  • Hookup wire

Suggested Reading

If you aren't familiar with the following concepts, you may want to check those out before moving ahead in this tutorial.

Hardware Assembly

When soldering your kit together, it's generally a good idea to check that you have all of the components first and then start soldering with the smallest components first.

We are going to start with the 1K Ohm resistor. Since resistors are not polarized, it doesn't matter which way we plug it into the board. Bend the legs at 90 degrees to the body of the resistor, and place one leg in each hole next to the 1K silkscreen on the top of the board. You should then solder the resistor legs on the side of the board opposite all of the silk screen. Make sure you get a good connection between the resistor legs and the board.

Resistor Soldered

Resistor soldered in the lower left corner of the board.

Once you have the resistor securely attached, it's time to add the red LED to the board. LEDs are polarized, so double check that you have the LED oriented correctly before soldering it down.

When looking at the LED, one leg should be longer than the other. This is the anode, or positive leg. The shorter leg, the cathode, should be placed in the hole closest to the flat edge of the LED silk screen on the board. This flat edge on the silk screen will also correspond to the flat edge of the LED casing as well. Again, this is important! If you solder in the LED backwards, it will not function!

LED Orientation

Make sure the LED is oriented properly *before* soldering it!

Flip the board over and solder the LED just like the resistor.

The next component to solder on is the switch. The switch is not polarized (just like the resistor), so you can place it in any orientation on the board. Place it in the box with the On/Off silk box, and solder the legs on the bottom of the board.

Switch Soldered

At this point, your board should look like this.

The next components you want to solder are the fuse clips. These clips are basically shaped pieces of conductive metal, but they still need to be oriented properly!! If you look at a single clip, one side of the U-shape will have two little curved-in pieces. These are designed to prevent the fuse from slipping out the end of the fuse clip. You will be pairing these up on the board (2 clips for each fuse), so they need to be oriented correctly to ensure that the fuse will actually fit in between them.

If you look closely at the silk screen on the board for the fuse clips, you will see one side of the square has a secondary line added. This is the side you should orient the curved bits towards.

Fuse clip orientation

Notice the secondary silk screen line on the same side as the curved edge on the clip.

Remember you need to be able to hold a fuse between each pair of clips, so be very careful when inserting them into the board. Double-checking before you solder them in will prevent frustrating rework time.

Fuse clip pair

These can be a bit finicky at staying in the holes while you solder them, so it may help to bend the tab out a bit on each leg of the clip before attempting to solder them. Also, keep in mind that these are just basically hunks of metal, so they will take a lot of heat from the soldering iron to get a properly flowed joint. The clip itself will also heat up, so make sure you don't accidentally touch it and burn yourself!

Once the fuse clips are in, you can either insert the fuses, or wait until you are done soldering, so they aren't in the way.

Inserted fuse

If the fuse slips out or won't stay inserted, take a pair of pliers and bend one side of the clip in towards the other. You'll want a good connection between the fuse clip and the fuse.

The last component you will be soldering onto the top of the board is the ATX connector. Make sure you carefully align all the pins and line up the edge of the connector with the edge of the board. The two plastic clips should also line up and snap into the vias on the board, to ensure the connector is oriented properly. Flip the board over and solder each of the pins. Make sure you don't bridge any of these - this connector can handle a large amount of current and a short could ruin your day.

ATX connector

Make sure you insert the ATX connector all the way into the board before soldering it down. The two white tabs should pop through the guide-holes.

Once you have all of the components soldered to the top of the board, it's time to connect the wires to the board. You will want to cut 8 2-inch pieces of wire (one for each barrel jack connector). I personally like to use red hook-up wire for the positive voltage lines and black hook-up wire for the ground voltage lines. Strip a bit of the coating off of each end of the wire. Once the wire is prepped, it's time to solder it.

Pre-cut wire

Prepped wire inserted into bottom of the board

To make the rest of the assembly go smoothly, you should connect the wire to the bottom of the board, meaning that you will be soldering on the top of the board. This should be opposite of all of the other soldering you have done up to this point.

Wires all soldered

So close to completion!

Once everything is soldered properly to the board, double check that you don't have any jumpers anywhere, and also make sure you clip any component legs that could potentially short out later.

It's time to add in your barrel jack connectors. You will want to unscrew the large nut from each jack, orient the jack in the hole in the board, and then reattach the nut on the bottom to secure the jack to the board. Again, this should follow the convention of red for positive voltages and black with ground connections.

Inserting barreljack

To connect your barrel jacks to your wires, you will want to unscrew the first small nut on the bottom of the barrel jack. Take the corresponding wire for that jack, and wrap it around the bottom of the jack. Then secure the wire in place by tightening back on the first nut to the jack.

Wire connected to barrel jack

It is extremely important at this step to ensure you connect your wires tightly to the jacks and to clip of any dangling ends. We really don't want these to short out once the system is powered!

Tightening nut on wire

Tighten those connections and trim those potential shorts.

The final step of the assembly is to attach the stand-offs. Keep in mind this step is optional, depending on how you will be using the board. If you intend to mount this into a case, you may not need the following steps. We do have a template file in the GitHub repo that you can use to mill or cut out a space for this board if you are so interested.

Insert a screw into the top of the board so the screw head lays flush on the same side as the components. Screw on the plastic standoff on the bottom of the board.

Standoff attachment

If you didn't already, now is the time to insert the fuses into the clips.

Your assembly is now complete!

Complete Kit

System Connection

Now that you have your Benchtop Supply soldered together, it's time to power it up! First, you will need to decide what system you are powering. For this example, we will be powering up a 4 RPM Standard Gear Motor. This motor can run from 3-12V, making it a great piece to simply test out several of the power rail connections on the Benchtop board.

Plug in the computer power supply's ATX connector into the Benchtop Power Supply. Since there is a power switch on the Benchtop Power Supply board, you can turn on the computer power supply and leave it on.

Place the bare wire ends into the barrel jacks of the appropriate voltage rail for your project. In our case, we are hooking up the motor to the 3.3V rail initially. Flip the power switch on the Benchtop board and you should see your motor spinning!

Resources and Going Further

Now that you understand the functionality of the Benchtop Power Supply board, you can use it to power many different projects and prototype many different components. We'd love to hear what you come up with!

If you have any feedback, please visit the comments or contact our technical support team at TechSupport@sparkfun.com.

Check out these additional resources for more information and other project ideas.