Adapting LilyPad Development Board Projects to the LilyPad ProtoSnap Plus

≡ Pages
Contributors: Gella

Board Comparison Chart

Below is a table that lists the components available on each of the boards. Note that in the ProtoSnap Plus, some boards have been removed. These can easily be hooked up again using the Expansion Ports on tabs A9, 10, and 11.

LilyPad Development Board Component LilyPad Development Board Pin LilyPad ProtoSnap Plus Pin Notes
LilyPad Vibe Board (+) 3 N/A The ProtoSnap Plus does not include a vibe board.
LilyPad Tri-Color LED Red LED: 9
Green LED: 11
Blue LED: 10
Red LED: 12
Green LED: 13
Blue LED: 14
The ProtoSnap Plus replaces a standalone tri-color LED with a built-in RGB LED on the LilyPad USB at the center of the board.
LilyPad Button A5 A4
LilyPad Switch 2 A9 2 is a hidden tab on the Development Board.
LilyPad Temperature Sensor (S) A1 N/A The ProtoSnap Plus does not include temperature sensor.
LilyPad Light Sensor (S) A6 A2 The ProtoSnap Plus uses an updated light sensor.
LilyPad Buzzer (+) 7 A3 7 is a hidden tab on the Development Board
5 LilyPad LEDs (+) White LED 1: 5
White LED 2: 6
White LED 3: A2
White LED 4: A4
White LED 5: A3
Yellow LED pair: A5
Red LED pair: 6
Green LED pair: A7
Blue LED pair: A8
The LilyPad ProtoSnap Plus replaces the 5 white LEDs with pairs of colored LEDs. It also includes an LED bar graph of white LEDs built into the LilyPad USB Plus on pins 15-20.