Vibe-O-Matic 3000

≡ Pages
Contributors: Nate

The Build

To build the Vibe-O-Matic, I needed three things:

  • Vibration
  • Sound
  • Light

Luckily, the bouncy seat that friends gave us (thank you Victoria!) had a small vibration motor attached.

Baby bouncy chair

The original vibration design used a single C cell battery (approximately 1.5V) with a simple ON/OFF slide switch. I removed the power switch and battery and used the MOSFET power control kit to control the motor via the Arduino at 5V. Since the DC motor was used to vibrate the seat, it did not matter what pin was used when connecting it to the "Device" side of the n-channel MOSFET's breakout board.

Vibration motor modified with MOSFET control

Vibration motor modified with MOSFET control

What does the motor do when run at 5V instead of the designed 1.5V? It runs a lot faster and a lot louder. Thankfully, the Arduino has PWM on a handful of pins so we are able to run the motor from 0 to 100% throttle. Therefore, if the vibration is too great (or the motor gets too warm), we can ramp down the power to an acceptable level. I ended up running the motor from about 40% to 80% power. Any higher and the boy gets even more weirded out.

Next, I soldered an Arduino Pro to the MP3 Player Shield. Note that the Arduino is mounted above the shield. It’s not mandatory that an Arduino go below a shield. I knew I was going to need to solder a variety of additional things like switches and buttons to the Arduino. It was easier for me to mount the MP3 shield below so I could see the pins I needed to access on the Arduino. After stacking, the following wired connections were made as shown in the following table.

Arduino Pro with MP3 Shield

5V Arduino Pro stacked on MP3 Shield with wired connections

Component Arduino Pro 5V/16MHz
Panel Mount Barrel Jack's Center Pin Barrel Jack VIN pin
Panel Mount Barrel Jack's Sleeve Pin Barrel Jack GND pin
N-Channel MOSFET Breakout Board: "C" Pin Pin 10
N-Channel MOSFET Breakout Board: "-" Pin GND Pin
N-Channel MOSFET Breakout Board: "+" Pin VIN Pin
APA102 Ground: GND "-" Pin Next to Barrel Jack Footprint
APA102 Data: D1 Pin Pin 5
APA102 Clock: C0 Pin Pin 4
APA102 Vcc: 5V "+" Pin Next to Barrel Jack Footprint
Go!: Momentary Push Button Pin Pin A0
Go!: Momentary Push Button Pin Pin A1
Vibe Mode: Rocker Switch Normally Closed Pin Pin A1
Car Mode: Rocker Switch Normally Open Pin Pin A2

I made a base board out of MDF to mount everything to. I had some extra paint around so I painted it (thinking a coat of paint would have a positive impact on my wife’s feelings about this whole endeavor). The speakers are attached with a couple of screws through the MDF into the plastic speaker housing. The enclosure and electronics were similarly secured with a couple screws.

MDF base board

MDF base board

The chair was then zip tied to the MDF. The individually addressable APA102 warm white LEDs had an adhesive backing like most strips do. But like most LED strips, this backing tends to wear out after a few days so I added hot-glue to various points on the LED strip to secure it.

Bouncy chair mounted to baseboard

Bouncy chair mounted to baseboard

The APA102 LEDs are controlled with the excellent FastLED library. The ‘Cylon’ example was modified to mimic car’s headlights illuminating the cabin as they pass on the left, right, and front.

Cylon LEDs emulating passing headlights

Cylon LEDs emulating passing headlights

Next, I recorded a 12 minute drive through my city with the windows down. If you listen to the track you can hear where a couple large diesel trucks pass by. It’s a pretty good track although it’s hard to pick up good road noises. At one point I envisioned using a light sensor, GPS, and accelerometer to properly record the light and vibration through the drive. At that same moment my son started to scream and I decided it was better to take the SISI (screw it, ship it) approach: the LEDs trigger every 30 seconds with a random right/front/left decision and the vibration motor changes to a new, random, vibration level (40 to 80% throttle) every 60 seconds.