Turn a Qwiic Ultrasonic Distance Sensor into a Garage Distance Sensor

≡ Pages
Contributors: -KJB-

How To Change Distance Parameters

Customizing your parking distance is easy with the SparkFun Qwiic Twist. Here's how to adjust the minimum and maximum distances for the green LED indicator:

  1. Initial Setup:
    • The default minimum distance is set to 50mm.
    • The default maximum distance is set to 250mm.
  2. Adjusting Parameters:
    • Use the Qwiic Twist to change either the minimum or maximum distance.
    • Rotate the Twist clockwise to increase the distance, or counterclockwise to decrease it.
  3. Switching Between Min and Max:
    • Click the Twist once to toggle between adjusting the minimum and maximum distances.
    • The OLED display will indicate which parameter you're currently modifying.
  4. Green LED Behavior:
    • The green LED will illuminate when your vehicle is within the set range.
    • Once you go past the minimum distance, the LED will turn off, signaling you to stop.
  5. Fine-Tuning:
    • Experiment with different min/max values to find your ideal parking position.
    • Remember, the minimum distance is your stopping point to avoid contact with the wall.

By adjusting these parameters, you can create a custom "sweet spot" for parking your vehicle, ensuring you park at the perfect distance every time. The intuitive twist-and-click interface makes it easy to modify your settings as needed.