Spectrum Shield Hookup Guide

This Tutorial is Retired!

This tutorial covers concepts or technologies that are no longer current. It's still here for you to read and enjoy, but may not be as useful as our newest tutorials.

View the updated tutorial: Spectrum Shield Hookup Guide (v2)

≡ Pages
Contributors: Toni_K

Hardware Overview

Audio Connections

Audio Jacks

The Spectrum Shield contains two audio stereo jacks on board. The first is the audio input jack (labeled "Input"). This allows you to input audio from any device -- such as an MP3 player, or cellular phone -- using a basic audio cable. This connection does not have to be used, as there is another option for adding audio input, at the "Audio In" headers, described below.

Audio Jacks

The second audio jack is the audio output, labeled "Output". This jack allows you to route the audio back out to a speaker or other audio system, after the sound levels have been processed by the Spectrum Analyzer ICs.

Audio In Header

For some projects, you may not be piping audio from a pre-processed source such as a cell phone. For users who want to use things like a MEMS Mic Breakout or the Sound Detector as an audio source, there are three header pins that allow you to connect bare wires to your shield.

Audio In Headers

These pins are as follows:

  • L = Left Audio Input
  • G = Ground Audio Input
  • R = Right Audio Input

With both the left and right inputs, you can use stereo devices on these headers.

MSGEQ7 ICs

The real power of this shield comes from the two MSGEQ7 ICs on the board. These are CMOS chips, which are seven band graphic equalizers.

MSGEQ7 ICs

Upon receiving an audio signal in, these ICs split the the spectrum into seven bands, splitting it at the following levels:

  • 63Hz
  • 160Hz
  • 400Hz
  • 1kHz
  • 2.5kHz
  • 6.25kHz
  • 16kHZ

For the visual learners, here's the frequency graph from the MSGEQ7 datasheet:

Frequency_Graph

Once the spectrum has been split into these ranges, each band is peak detected and multiplexed. The DC output is a representation of the amplitude of each frequency band. Using the strobe and reset pins on the ICs allows the user to select the DC peak output.

RedBoard Connections

There are 4 main pins that connect the Spectrum Shield with the Arduino/RedBoard or other microcontroller.

Analog Pins - There are two analog pins connected to the MSGEQ7 ICs. Analog 0 is the DC output from the first IC, while Analog 1 is the DC output from the second.

Control Pins - The MSGEQ7 control pins are Strobe and Reset. These are connected to D4 and D5, respectively. In order to enable the Strobe pin, you must pull the Reset pin LOW. To reset the entire multiplexer, pull the Reset pin HIGH.

The Strobe pin, once activated, cycles through each of the channels. After the initial pulse, it starts at 63Hz, pulses each channel until 16kHz, and then repeats, starting back at 63Hz. The DC output for each channel will follow the Strobe pulse.

Remember: The reset line for the MSGEQ7 IC is **not** the same as the "Reset" push button that resets the entire system (RedBoard + Shield).

Reset Button

The reset button allows you to reset your Arduino/RedBoard while the shield is inserted. Holding the reset button will pull the reset pin of the ATMega328 low, allowing a system reset. This will restart any sketches currently running on the microcontroller.

Reset Button