SparkFun Serial Basic CH340C Hookup Guide

≡ Pages
Contributors: Elias The Sparkiest

Serial Basic Overview

The pinout of the Serial Basic mimics the common DTR/RX/TX/VCC/CTS/GND pinout found on hundreds of FTDI-to-USB derivatives.

Pin LabelInput/OutputDescription
DTROutputData Terminal Ready, Active Low
RXIInputSerial Receive
TXOOutputSerial Transmit
VCCSupply OutputPower supply 3.3V (Default) or 5V
CTSInputClear To Send, Active Low
GNDSupply OutputGround (0V) supply

USB-C

USB-C gives you the potential of more power than the previous generation of USB. USB-C is used to power everything from laptops to low powered micro controllers and has the amazing capability of being reversible.

This image shows the topside of the product with the USB-C connector highlighted.

LEDs

The two LEDs on the board are connected to TX (Green) and RX (Yellow) and are correctly aligned to the silk header labels: RXI and TXO . This is a quick and handy way to see the serial traffic.

An image of the Serial Basic with the RX and TX LEDs highlighted.

Alignment Markers

The GRN and BLK silk in the corners opposite of the USB-C connector, is there to help you align the board properly with products that use these same orientation indicators.

This picture shows the alignment silk at the two corners of the board nearest the female header labeled 'Black' and 'Green'.

The Serial Basic mates seamlessly with products that use the standard serial connection. If you see a board with the BLK and GRN labels, then you know it will be compatible with the Serial Basic.

nRF52832 Breakout

See the GRN and BLK labels on this nRF52832 Breakout?

Where did GRN and BLK come from? Way back in 2008, when we created the Arduino Pro Mini, we needed to have a pinout to allow serial bootloading. At the time, the best USB to TTL Serial device was the FT232 Cable. Its unpolarized connector could be flipped either way so we added the words GRN and BLK to the PCB to let folks know how to line up the colored wires. The practice stuck! Now, many boards use this standard.

The old FTDI Cable

The cable with colored wires

Voltage Selection Jumper

There is a jumper on the underside of the board that controls the output voltage on the VCC pin. By default, the board outputs 3.3V and has 3.3V signals.

This image shows the underside of the product with the USB-C facing right. It highlights the three way jumper near the right edge where the top jumper is labeled 3.3V and the bottom jumper is labeled 5V.

There is a small trace connecting the middle pad and the top pad labeled 3.3V.

When the jumper is set to 3.3V, the board uses an on board 3.3V regulator capable of sourcing 600mA. If you attempt to pull more than 600mA, the regulator will go into short-circuit shutdown where it will only output 150mA.

You can change the board's output and signal to 5V by cutting the trace between the center and 3.3V labeled pad and putting solder on the center and 5V labeled pad. This will change the board's output to 5V on the VCC pin with 5V signals.

This image shows the same jumper but the small trace connecting 3.3V is cut and solder has been added to the 5V side of the three way jumper.

When the jumper is set to 5V, the board will source as much power as your USB port will provide. With USB-C this can be up to 1.5Amps but depending on what is providing the power and the capabilities of your cable, you can get up to 3 Amps.