SparkFun Humidity Sensor Breakout - SHTC3 (Qwiic) Hookup Guide

≡ Pages
Contributors: El Duderino

Hardware Assembly

Using the Qwiic system, assembling the hardware is simple. All you need to do is connect your SparkFun Humidity Sensor Breakout - SHTC3 (Qwiic) to your chosen development board with a Qwiic cable or adapter cable. Otherwise, you can use the I2C pins broken out if you prefer. If you are not using a Qwiic-enabled board, make sure your input voltage and logic are either running at 3.3V or you are running both controller and SHTC3 at the same logic level.

SHTC3 connected to a RedBoard Qwiic

If you prefer to use the PTH pins broken out on the Humidity Sensor you will need to either solder to them or, if you want a temporary connection for prototyping, these IC Hooks are a perfect option to make that connection. If you are not familiar with through-hole soldering, take a look at this tutorial:

How to Solder: Through-Hole Soldering

September 19, 2013
This tutorial covers everything you need to know about through-hole soldering.

With our SHTC3 connected to our microcontroller we can move on to writing some code to start monitoring temperature and humidity.