SparkFun Blocks for Intel® Edison - ADC
This Tutorial is Retired!
This tutorial covers concepts or technologies that are no longer current. It's still here for you to read and enjoy, but may not be as useful as our newest tutorials.
Contributors:
SFUptownMaker,
CaseyTheRobot,
HelloTechie
Board Overview
ADC Block Functional Diagram
Single Inputs - Four single inputs are available. The reference voltage for each is produced internal to the ADC.
Differential Pairs - Use two inputs to create a differential pair. Useful for eliminating noise in some sensors.
I2C Address Select - Apply solder to (only) one of the four jumpers to select the address.
Expansion Header - The 70-pin Expansion header breaks out the functionality of the Intel Edison. This header also passes signals and power throughout the stack. These function much like an Arduino Shield.