Roshamglo Hookup Guide

≡ Pages
Contributors: Alex the Giant

Hardware Overview

Roshamglo labels

The Roshamglo uses the following:

  • ATtiny84
  • IR LED
  • IR receiver with built in 38kHz demodulator
  • USB programming
  • Programmable red and green LED
  • A switch for power
  • 5-way switch for input
  • Reset switch
  • 6x AAA PTH battery clips
  • 3x AAA batteries for power

The brains behind the Roshamglo is an ATtiny84, a light weight Arduino compatible microcontroller. The ATtiny84 comes with the following:

  • 8kB of flash memory for our program (~6kB after the bootloader is installed)
  • 512B of SRAM, which stores our variables used in our program
  • 512B of EEPROM
  • 12 IO pins MAX (the Roshamglo breaks out 9 of these pins)
  • 10-bit analog to digital converter which can be used on 8 pins

For details about what each pin is able to do, refer to the table below.

PinAnalog or DigitalAdditional UsesRoshamglo Uses
0Both Analog Reference5-way switch down
1Both --5-way switch right
2Both --5-way switch up
3Both --IR Receiver
4Both SCK, SCL5-way switch left
5Both MISO, PWMIR LED
6Both MOSI, SDA, PWM5-way switch center
7Both PWMGreen LED
8Digital PWMRed LED
Missing from the list, are digital pins 9 and 10. The bootloader, uses these two pins for USB programming.

Jumpers and Pins Highlighted

Each of these pins have been broken out to edge of the board to make customization easy! If you would like to use any of these pins for something other than what it's currently connected two, we provided jumpers that can easily be cut with a hobby knife. The only pins that do not have a jumper on them are the pins used for the 5-way switch. The pins for the switch use the ATtiny's internal pull up resistors, so as long as the switch is not closed, the pin can be configured in any way you'd like without having to cut traces.

One important feature missing

If you hadn't noticed in the pin description, there was no mention of RX or TX pins. This is because unfortunately the ATtiny84 doesn't have a hardware UART. The UART is used for serial communication, whether it's for programming, or printing messages to the serial window. You might be thinking "But doesn't the USB connector provide communication between the ATtiny and computer?", and you're right; it does. To keep the bootloader size as small as possible, the bootloader only allows for USB programming. For serial debugging, you'll need a USB cable and a USB-to-Serial adapter, and Software Serial library to send messages to a computer. You can learn more about serial communication here.