Robot Quickstart!

≡ Pages
Contributors: Miskatonic

Introducing the Hardware

Introducing the H-Bridge

alt text

WARNING: You will be using voltage that may be higher than the limit of the circuitry on your RedBoard allows! Make sure you keep motor voltage (MV) isolated from other circuitry! Accidentally using MV to power other circuitry may cause irreparable damage to your RedBoard!

The Toshiba TB6612FNG is actually a dual H-bridge IC. This means it has two full H-bridge circuits built into a little package, allow- ing you to control the two motors on your robot with a single board. The H-bridge distinguishes the two motors as A and B, as you can see on the underside of the board in Figure 8-6. To control each H-bridge circuit, you use three signal wires: two for direction and one for speed. You can buy the board either with or without pins already sol- dered on, so if you want to save yourself the trouble of soldering, make sure you get the presoldered board (ROB-13845). If you have the board without header pins already soldered on (ROB-09457), it’s not a problem, but you’ll need to solder male headers onto the pins; for soldering instructions, see “How to Solder” on page 302. In either case, before you start building this project you should have a board that looks like first picture in this tutorial.

alt text

Hookup Table

1 Motor voltage supply
2 Chip supply voltage
3 Ground 1
4 AO1 motorA connection
5 AO2 motorA connection
6 BO2 motorB connection
7 BO1 motorB connection
8 Ground(GND)
9 Ground(GND)
10 PWMB (MotorB Speed)
11 BIN2(MotorB2 DIR2)
12 BIN2(MotorB2 DIR1)
13 STBY
14 AIN1(MotorA DIR1)
15 AIN2(MotorA DIR2)
16 PWMA (MotorA Speed)

Geared Hobby Motor

The basic hobby motor is great for simple mechanisms like spinning fans, but it doesn’t offer a lot of torque (rotational force). In this project, we want to use a motor to move the entire project around, so we need to use a geared motor—a motor that’s attached to a gearbox.

alt text

A gearbox essentially converts mechanical rotations into torque. This gearbox has a 48:1 gear reduction, which means 48 rotations of the motor equal one rotation of the output shaft. This slows down the motor by a factor of roughly 1/48 and results in a multiplication of the torque by a factor of 48. Basically, the output speed is slower, but the torque is a lot higher.