Comments: RETIRED - BadgerHack

Pages

Looking for answers to technical questions?

We welcome your comments and suggestions below. However, if you are looking for solutions to technical questions please see our Technical Assistance page.

  • Mike Szczys / about 12 years ago / 2

    This is a fantastic way to get kids interested in hardware. Well done (and thanks for giving me a kit when I stopped by the booth)!

    • Thanks! Glad you liked it :) Any plans to make it do other stuff?

      • mercury2010 / about 12 years ago / 1

        I'm trying to attach a parallax gyroscope via i2c but can't get any of that code to give me a response. SDA on A4 and SCL on A5? correct? (what other board is this closestly related to?)

        btw, tell the crew, passing out an led array and INCLUDING charlieplexing with this was INGENIOUS. the one thing that was crippling me for months was not having enough pins to control a 4 digit alpha numeric display for some feedback... and / or no multiplexer. and here, Its got all of that built right in (basically)

        • Correct, SDA is A4 and SCL is A5. The board is most like the Pro Mini (the pinout is the same). However, keep in mind that it has a customized Arduino bootloader to let it run at 4 MHz and all the way down to 1.8 V for the microcontroller. It looks like the gyro you're talking about needs at least 2.7 V. Are you trying to run it from batteries or USB power?

          And I'll tell the team that the LED array is working out great :)

  • kwan3217 / about 11 years ago * / 1

    I got one of these at AVC and I really like it! However, I can't find the exact eagle files for it. I found something close on Github, but it isn't exactly the one I have. It at least has a JST connector instead of a two-pin 0.1 header as I received and as appears in the photos in this tutorial.

  • co_buckfast / about 11 years ago / 1

    In the section "Your First Badger Hack," you should place a comment above the first delay statement telling users what that delay is for. Right after printing out "Hello world," we changed the string to something longer and were confused for a bit why only so much text scrolled by before disappearing.

    Also, the comment above the scrollText call says to scroll 2 times but the parameter passed is a 1.

    We got copies at the 2015 AVC workshop and really like them. I expect they might be offered for sale at some point. Some better documentation of the Sparkfun_LED_8x7 (so you don't have to open up the header or source files) just to play around would be much appreciated by casual users.

    • Thanks for the feedback! I added comments to the scrolling text, so hopefully it will be a bit more clear. We're working on making some of these pieces products, at which point there will be full hookup guides for them (e.g. the LED array).

  • whotookdman977 / about 11 years ago / 1

    I have Arduino IDE v.1.6.4 and replacing the boards.txt file does nothing. Any ideas?

    • co_buckfast / about 11 years ago / 1

      I have v.1.6.3 and replacing the boards.txt file did work. Maybe that helps in identifying the issue and solution.

    • Arduino has changed how they handle board definition files in the last few revisions since they've added a board manager. For now, I recommend just downloading 1.6.1 and using that for the Badgers. I am working on an update to the Badgers that will play nicely with the latest Arduino (e.g. 1.6.3 and 1.6.4).

      EDIT: You can run 1.6.1 and 1.6.4 side by side in your computer. It should not affect anything. I have 1.0.6, 1.6.1, 1.6.3, and 1.6.4 all installed next to each other. I find that they keep changing stuff on a regular basis, and it keeps breaking old libraries.

  • JN_Austin / about 11 years ago / 1

    I'm using one of the SXSW boards to communicate with a GPS and SPI memory. I have got some sample code working but wondered about the 4Mhz clock. Will the slow speed affect the micros() command? I uderstand the following;

    "Micros() Returns the number of microseconds since the Arduino board began running the current program. This number will overflow (go back to zero), after approximately 70 minutes. On 16 MHz Arduino boards (e.g. Duemilanove and Nano), this function has a resolution of four microseconds (i.e. the value returned is always a multiple of four). On 8 MHz Arduino boards (e.g. the LilyPad), this function has a resolution of eight microseconds."

    Does this mean the 4Mhz Badgerback board would have a resolution of 16 microseconds?

  • Member #491132 / about 11 years ago / 1

    I'm using this for a project, where can I find info about the pinsouts and such?

  • Panos Br / about 11 years ago / 1

    Hey Sparkfun! Are you going to sell the badgerhack through your site?

  • stej / about 12 years ago / 1

    Is there a way to get one without going to SXSW?


If you've found an issue with this tutorial content, please send us your feedback!