Qwiic OpenLog Hookup Guide

≡ Pages
Contributors: Nate, Toni_K, Ell C, Englandsaurus

Configuration File

The configuration file is not as relevant with the updated Qwiic OpenLog as it was with its predecessor. When you open the config file, you will see the I2C address, escape character, the number of escape characters, and the mode. You can edit the I2C address and the mode, but ignore the escape character and number of escape characters. Here's what you will see when opening the config.txt file in a text editor. As you can see, the i2c_address is 42. This is the default address of the Qwiic OpenLog in decimal form. Converting the value, this matches our default address which is 0x2A.

language:bash
42,26,3,0
i2c_address,escape,esc#,mode