Qwiic HAT for Raspberry Pi Hookup Guide

≡ Pages
Contributors: Englandsaurus

Introduction

This Qwiic HAT for Raspberry Pi is the quickest and easiest way to utilize SparkFun's Qwiic ecosystem while still using that Raspberry Pi that you've come to know and love. This Qwiic HAT connects the I2C bus (GND, 3.3V, SDA, and SCL) on your Raspberry Pi to an array of Qwiic connectors. It also has a few important pins on the Raspberry Pi broken out for easy access. Since the Qwiic system allows for daisy chaining (as long as your devices are on different addresses), you can stack as many sensors as you'd like to create a tower of sensing power!

SparkFun Qwiic HAT for Raspberry Pi

DEV-14459
$6.95

Required Materials

To follow along with this hookup guide, you will need any Raspberry Pi with 2x20 male headers.

Raspberry Pi 3 B+

DEV-14643
$43.50

A Pi Zero W will also work but you will need to make sure to solder some male headers to it.

Raspberry Pi Zero W

DEV-14277
$16.50

GPIO Header - Male (PTH, 0.1in., 2x20-Pin)

PRT-14275
$1.10

Now you probably didn't buy the Qwiic HAT if you didn't have any Qwiic products to use with it, right? If you don't have any Qwiic products, the following might not be a bad place to start.

SparkFun Qwiic Adapter

DEV-14495
$1.60

SparkFun GPS Breakout - XA1110 (Qwiic)

GPS-14414
$35.95

SparkFun Spectral Sensor Breakout - AS7262 Visible (Qwiic)

SEN-14347
Retired

SparkFun Environmental Combo Breakout - CCS811/BME280 (Qwiic)

SEN-14348
Retired

Finally, you'll need our handy Qwiic cables to easily connect sensors to your Qwiic HAT. Below are a few options.

Qwiic Cable - 50mm

PRT-14426
Retired

Qwiic Cable - 100mm

PRT-14427
Retired

Qwiic Cable - 200mm

PRT-14428
Retired

Qwiic Cable - 500mm

PRT-14429
Retired

Required Setup Tools

As a desktop, these devices are required:

Suggested Reading

If you aren't familiar with the Qwiic system, we recommend reading here for an overview.

Qwiic Connect System
Qwiic Connect System

We would also recommend taking a look at the following tutorials if you aren't familiar with them.

I2C

An introduction to I2C, one of the main embedded communications protocols in use today.

Serial Terminal Basics

This tutorial will show you how to communicate with your serial devices using a variety of terminal emulator applications.