Qwiic Distance Sensor (RFD77402) Hookup Guide

≡ Pages
Contributors: Englandsaurus

Hardware Overview

Let's first check out some of the characteristics of the RFD77402 sensor we're dealing with, so we know what to expect out of the board.

CharacteristicRange
Operating Voltage3.3V
Current7 mA average at 10Hz
Measurement Range~50mm to 2,000mm
Precision+/-10%
Light Source850nm VCSEL
I2C Address0x4C
Field of View55°
Field of Illumination23°
Max Read Rate10Hz (We've seen up to 20Hz in practice)

Pins

The following table lists all of the RFD77402's pins and their functionality.

PinDescriptionDirection
GNDGroundIn
3.3VPowerIn
SDADataIn
SCLClockIn
INTInterrupt, goes low when data is ready.Out

Optional Features

The RFD77402 breakout has onboard I2C pull up resistors; if multiple sensors are connected to the bus with the pull-up resistors enabled, the parallel equivalent resistance will create too strong of a pull-up for the bus to operate correctly. As a general rule of thumb, disable all but one pair of pull-up resistors if multiple devices are connected to the bus. If you need to disconnect the pull up resistors they can be removed by removing the solder on the corresponding jumpers highlighted below.

Pull Up Resistors Jumper