Qwiic Ambient Light Sensor (VEML6030) Hookup Guide

≡ Pages
Contributors: Elias The Sparkiest

Introduction

The SparkFun Ambient Light Sensor (VEML6030) is an I²C enabled ambient light sensor with high sensitivity and high accuracy. It reads ambient light in Lux and boasts a number of nice features including: the ability to set high and low thresholds for an optional interrupt, power saving features that enable single digit micro-amp current draw, and a readable range from zero to 120,000 Lux. We've also written an Arduino library that gives full access to all features and includes example code demonstrating all its' abilities. Follow along and let's learn about all its features and how to use them!

SparkFun Ambient Light Sensor - VEML6030 (Qwiic)

SEN-15436
$5.95

Required Materials

To follow along with the example code used in this tutorial, you will also need the following materials. You may not need everything though depending on what you have. Add it to your cart, read through the guide, and adjust the cart as necessary.

If you need different size Qwiic cables we offer a kit that contains many sizes but we also carry them individually as well:

SparkFun Qwiic Cable Kit

KIT-15081
$12.95

Qwiic Cable - Breadboard Jumper (4-pin)

PRT-14425
Retired

Qwiic Cable - 100mm

PRT-14427
Retired

Qwiic Cable - 500mm

PRT-14429
Retired

Suggested Reading

If you aren't familiar with the Qwiic system, we recommend reading here for an overview.

Qwiic Connect System

We would also recommend taking a look at the following tutorials if you aren't familiar with them.

I2C

An introduction to I2C, one of the main embedded communications protocols in use today.

How to Work with Jumper Pads and PCB Traces

Handling PCB jumper pads and traces is an essential skill. Learn how to cut a PCB trace, add a solder jumper between pads to reroute connections, and repair a trace with the green wire method if a trace is damaged.

RedBoard Qwiic Hookup Guide

This tutorial covers the basic functionality of the RedBoard Qwiic. This tutorial also covers how to get started blinking an LED and using the Qwiic system.

Hardware Overview

Power

You can provide 3.3V through the Qwiic connector on the board or through the 3V3 labeled pin on the through hole header. When you correctly power the board, the on-board red power LED will turn on.

This image shows a picture of the top of the product with the Qwiic connectors and two left most through holes highlighted.

LED

There is one red LED on the product that will turn on when power is supplied to the board. You can disconnect this LED by cutting the jumper on the underside of the product labeled LED, see Jumpers below.

This shows an image of the top of teh board with the top left Power LED highlighted.

Qwiic Connector or I2C Pins

There are two Qwiic connectors on the board to easily connect to the sensor via I2C. Another option is to solder directly to the I2C plated through holes on the side of the board. We have many Qwiic sensors and Qwiic enabled micro-controllers. Check out our Qwiic Ecosystem page to get a glimpse of what else we have to offer.

This shows an image of the product with the Qwiic connectors again highlighted but now the two pins labeled SDA and SCL for I2C data lines are now hightlighted as well.

Interrupt Pin

A nice feature on the SparkFun Ambient Light sensor is its ability to set both LOW and HIGH thresholds that triggers an interrupt on the product. For example, we can know when the light in a room falls below a certain amount and conversely when the light comes back on! You don't have to settle for just the hardware interrupt though. We also have a software solution, check out the interrupt example code below.

This image shows a picture of the product the right most interrupt through hole labeled "INT" highlighted.

Jumpers

There are three jumpers on the underside of this board. Starting in the lower left is a triple jumper labeled I2C that connects pull-up resistors to the I²C data lines. If you're daisy chaining many I²C devices together than you may need to consider cutting these traces.

I2C Jumper

To the right of that is the address jumper labeled ADR that allows you to select the SparkFun Ambient Light Sensor's other I²C address: 0x10. By default your SparkFun Ambient Light Sensor is shipped with the I²C address 0x48.

Address Jumper

Finally the jumper in the upper right is the LED jumper which can be cut to disconnect the on board power LED.

LED Jumper

Gain and Integration Time Settings

What does gain and integration time mean? You can think of gain as an electronic mechanism to amplify a weak signal. If you're in a dark room with very little light, the sensor needs a way to amplify the weak light source to get accurate lux calculations and the gain is what give is it's oomph. Likewise, Integration time is the amount of time the sensitive photo diodes within the sensor absorb light before beginning its' Lux calculation. Both of these together are necessary for sensing in a dark room, but what if it was really bright outside?! Now there's so much light in the envinronment that you actually want to scale down the electronic's response to that saturation so you need a lower gain. And since there's so much light, the photo diodes don't need to be exposed long to get what they need to make the calculations, so a lower integration time is also needed.

The SparkFun Ambient Light Sensor can detect ranges of light in Lux from zero to 120,796! That's a gigantic range from dark to direct sun in the middle of the day. To accomplish this you have to set the Gain and Integration Time settings. This is trivial with the Arduino Library we've written and we'll walk you through it below in Example1 Ambient Light Basics. With each setting gives you a range of light that you can read. Check out the table below to see what's capable at each possible setting. Notice that slower integration and higher gain gives you a smallest range of (0->236) but the highest resolution (0.0036 lux/bit).

The datasheet recommends that you use a setting of 1/4 (.25) or 1/8 (.125) unless the Ambient Light Sensor is going to sit behind dark glass. This will help to prevent over saturation of the photodiodes within the sensor.

Maximum Light Detection Range: Lux

Integration Time (milliseconds) GAIN 2 GAIN 1 GAIN 1/4 GAIN 1/8
800 236 472 1887 3775
400 472 944 3775 7550
200 944 1887 7550 15099
100 1887 3775 15099 30199
50 3775 7550 30199 60398
25 7550 15099 60398 120796

Resolution: Lux/Bit

Integration Time (milliseconds) GAIN 2 GAIN 1 GAIN 1/4 GAIN 1/8
800 0.0036 0.0072 0.0288 0.0576
400 0.0072 0.0144 0.0576 0.1152
200 0.0144 0.0288 0.1152 0.2304
100 0.0288 0.0576 0.2304 0.4608
50 0.0576 0.1152 0.4608 0.9216
25 0.1152 0.2304 0.9216 1.8432

Power Save Modes

Another cool feature of the SparkFun Ambient Light Sensor is its ability to run at extremely low currents. Power save modes should be used when you're continuously reading ambient light data. For example, if you're going to gather ambient light data every second, why not use a power save mode and save battery life? There are four power save modes that can be enabled with integration times of 100ms and above. Below is a table showing the power save mode, the current draw, and it's refresh rate. Check out Example 4 in the Arduino Library to see how to set it up and use the table below as a reference.

Note the Refresh Time is the time needed for a new reading to be ready. Make sure there is a delay in your code of at least this length between readings to ensure you're getting new data.
Integration Time Power Save Mode Refresh Time (milliseconds) Current Draw (microamperes) Resolution (lx/bit)
100 1 600 8 0.0288
100 2 1100 5 0.0288
100 3 2100 3 0.0288
100 4 4100 2 0.0288
200 1 700 13 0.0144
200 2 1200 8 0.0144
200 3 2200 5 0.0144
200 4 4200 3 0.0144
400 1 900 20 0.0072
400 2 1400 13 0.0072
400 3 2400 8 0.0072
400 4 4400 5 0.0072
800 1 1300 28 0.0036
800 2 1800 20 0.0036
800 3 2800 13 0.0036
800 4 4800 8 0.0036

Rounding Errors?!

Later on when you read back an interrupt threshold, you may notice that the interrupt lux values are off by one in some cases. This is because of the inherent rounding error with the Ambient Light Sensor. The final Lux value is calculated by multiplying the value of the bits that represent the ambient light by a decimal number (0.2304 for example). This decimal number is rounded to a whole number (e.g. 19.97 becomes 19) because the sensor does not care about fractions of a Lux. I chose to read back the rounded number because that's the interpreted value of the ambient light sensor and what is stored in its' registers.

Hardware Hookup

This will be an easy one thanks to the Qwiic connectors. Take one end of a Qwiic cable and plug it into your RedBoard Qwiic Board and then take the other end and plug it into the SparkFun Ambient Light Sensor.

This image shows a picture of the SparkFun Ambient Light Sensor connected to a Redboard Qwiic by a Qwiic cable.

Arduino Library

Note: This example below assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using Arduino, please review our tutorial on installing the Arduino IDE. If you have not previously installed an Arduino library, please check out our installation guide.

If you've never connected an CH340 device to your computer before, you may need to install drivers for the USB-to-serial converter. Check out our section on How to Install CH340 Drivers for help with the installation

We've written a library to make it even easier to get started with the SparkFun Ambient Light Sensor. The library will give you the full functionality of the sensor and provides example code to get the most our of your project. You can obtain these libraries through the Arduino Library Manager by searching SparkFun Ambient Light Sensor. The second option is to download the ZIP file below from its GitHub repository to manually install.

Example 1: Ambient Light Basics

In this first example, we'll get you comfortable with gathering ambient light and setting two vital properties of the sensor's ability to read light: the gain and the integration time. These two properties determine the resolution (accuracy) of the reading and the available ranges of light that you can read! For example, a gain of 1/8 and 800ms integration time cannot read anything above 3775 Lux. This means you'll max out your sensor outdoors but would be a proper setting for dim rooms due to it's higher resolution.

At the top of the example we have three variables gain, time, and luxval. The first two hold the value for the gain and integration time settings mentioned above. Gain settings can be: 2, 1, 1/4, and 1/8; typically 1/4 gain will capture everything you need with good resolution. Possible integration times can be 800, 400, 200, 100, 50, 25 and by default the sensor is set to 100; times are in milliseconds. Check the Gain and Integration Time table above under Hardware Overview to see maximum illumination capabilities and resolution for every setting.

If you have any doubt with which settings to pick, just keep the example code's default settings: a gain of 1/4 (0.125) and an integration time of 100ms. This will give you a range of up to 15,000 Lux with a decent resolution!

language:c
#include <Wire.h>
#include "SparkFun_VEML6030_Ambient_Light_Sensor.h"

#define AL_ADDR 0x48

SparkFun_Ambient_Light light(AL_ADDR);

// Possible values: .125(1/8), .25(1/4), 1, 2
// Both .125 and .25 should be used in most cases except darker rooms.
// A gain of 2 should only be used if the sensor will be covered by a dark
// glass.
float gain = .125;

// Possible integration times in milliseconds: 800, 400, 200, 100, 50, 25
// Higher times give higher resolutions and should be used in darker light. 
int time = 100
long luxVal = 0; 

In the setup, we call light.begin() to check if we can communicate with the SparkFun Ambient Light Sensor. Next, we call the light.setGain() and light.setIntegTime() functions giving them the variables holding the gain and time values above. Next we'll read back those values to make sure that they were set correctly. That's it! We're now set to read some light!

language:c
void setup(){

  Wire.begin();
  Serial.begin(115200);

  if(light.begin())
    Serial.println("Ready to sense some light!"); 
  else
    Serial.println("Could not communicate with the sensor!");

  // Again the gain and integration times determine the resolution of the lux
  // value, and give different ranges of possible light readings. Check out
  // hoookup guide for more info. 
  light.setGain(gain);
  light.setIntegTime(time);

  Serial.println("Reading settings..."); 
  Serial.print("Gain: ");
  float gainVal = light.readGain();
  Serial.print(gainVal, 3); 
  Serial.print(" Integration Time: ");
  int timeVal = light.readIntegTime();
  Serial.println(timeVal);

}

One thing to keep in mind is that you need to set a delay() in between readings. The Integration Time is the amount of time that the sensor uses to fill its' sensitive components with light. If you set an integration time of 100ms then make sure you're delay is at least that long. A longer integration time will need a longer delay.

language:c
void loop(){

  luxVal = light.readLight();
  Serial.print("Ambient Light Reading: ");
  Serial.print(luxVal);
  Serial.println(" Lux");  
  delay(1000);

}

Example 2 and 3: Ambient Light Interrupt

The SparkFun Ambient Light Sensor can issue an interrupt whenever the ambient light readings cross high or low thresholds. In this example, we'll talk about setting those thresholds and reading when those thresholds have been crossed in two different ways:

  • the on-board hardware interrupt pin labeled INT
  • through software monitoring

The code for both Example 2 and 3 only differ in the main loop() and these differences are highlighted under Example 2 - Hardware Interrupt and Example 3 - Software Interrupt sections below.

Again as in example one, at the top we see the gain, time and luxVal variables. The gain and integration times are vital for setting the tolerance for light and resolution of your sensor - see the Gain and Integration Time table under Hardware Overview above. The luxVal variable holds the ambient light readings further down in the code. Just below we see the interrupt settings lowThresh, highThresh and numbValues. The first two set the low and high threshold variables that will trigger the interrupt when the ambient light crosses the given values. The last variable is the number of times a value must cross a threshold to trigger an interrupt. I have the variables set to 20 Lux for the lower end, 400 Lux for the upper end, and that an interrupt must be issued after the ambient light crosses one of these thresholds once.

language:c
#include <Wire.h>
#include "SparkFun_VEML6030_Ambient_Light_Sensor.h"


// Close the address jumper on the product for addres 0x10.
#define AL_ADDR 0x48

SparkFun_Ambient_Light light(AL_ADDR);

// Possible values: .125, .25, 1, 2
// Both .125 and .25 should be used in most cases except darker rooms.
// A gain of 2 should only be used if the sensor will be covered by a dark
// glass.
float gain = .125;

// Possible integration times in milliseconds: 800, 400, 200, 100, 50, 25
// Higher times give higher resolutions and should be used in darker light. 
int time = 100;
long luxVal = 0; 


// Interrupt settings. 
long lowThresh = 20; 
long highThresh = 400; 
int numbValues = 1;

// Interrupt pin
int intPin = 3;
// -- OR -- if not using interrupt pin:
int interrupt;

Again, as in the first example, we start communication with the sensor with light.begin(), set the gain (light.setGain()) and integration time settings (light.setIntegTime()), and read them back by printing them out to the serial monitor with the respective read functions. But just below we see where we set the two thresholds. First the low threshold with light.setIntLowThresh() and then the high threshold with light.setIntHighThresh(), giving these functions the values we set in the variables above. We then read those settings back to make sure that they're set correctly.

Now we set how many values will need to cross the threshold with the light.setProtect() function call and read it back. This setting is optional and defaults to one. Finally, we enable the interrupt with light.enableInt(). While the sensor knows our thresholds it does not quite know we want the interrupt to be enabled until we tell it to.

language:c
void setup(){

  Wire.begin();
  Serial.begin(115200);
  pinMode(intPin, INPUT);

  if(light.begin())
    Serial.println("Ready to sense some light!"); 
  else
    Serial.println("Could not communicate with the sensor!");

  // Again the gain and integration times determine the resolution of the lux
  // value, and give different ranges of possible light readings. Check out
  // hoookup guide for more info. The gain/integration time also affects 
  // interrupt threshold settings so ALWAYS set gain and time first. 
  light.setGain(gain);
  light.setIntegTime(time);

  Serial.println("Reading settings..."); 
  Serial.print("Gain: ");
  float gainVal = light.readGain();
  Serial.print(gainVal, 3); 
  Serial.print(" Integration Time: ");
  int timeVal = light.readIntegTime();
  Serial.println(timeVal);

  // Set both low and high thresholds, they take values in lux.
  light.setIntLowThresh(lowThresh);
  light.setIntHighThresh(highThresh);
  // Let's check that they were set correctly. 
  // There are some rounding issues inherently in the IC's design so your lux
  // may be one off. 
  Serial.print("Low Threshold: ");
  long lowVal = light.readLowThresh();
  Serial.print(lowVal);
  Serial.print(" High Threshold: ");
  long highVal = light.readHighThresh();
  Serial.println(highVal);

  // This setting modifies the number of times a value has to fall below or
  // above the threshold before the interrupt fires! Values include 1, 2, 4 and
  // 8. 
  light.setProtect(numbValues);
  Serial.print("Number of values that must fall below/above threshold before interrupt occurrs: ");
  int protectVal = light.readProtect();
  Serial.println(protectVal);

  // Now we enable the interrupt, now that he thresholds are set. 
  light.enableInt();
  Serial.print("Is interrupt enabled: ");
  int enabInt = light.readIntSetting();
  if( enabInt == 1 )
    Serial.println("Yes"); 
  else
    Serial.println("No");

  Serial.println("-------------------------------------------------");

  // Give some time to read our settings on startup.
  delay(3000);
}

Example 2: Hardware Interrupt

Now let's read some light! Since we're just using a hardware interrupt we have a pin attached to PIN 3. When the ambient light reading passes either threshold the pin will go LOW. When an interrupt fires we check to see which threshold was crossed and print it out in the serial monitor.

language:c 
void loop(){

  luxVal = light.readLight();
  Serial.print("Ambient Light Reading: ");
  Serial.print(luxVal);
  Serial.println(" Lux");  

  if (digitalRead(intPin) == LOW){
    int intVal = light.readInterrupt();
    if (intVal == 1)
      Serial.println("High threshold crossed!");
    else if (intVal == 2){
      Serial.println("Low threshold crossed!");
    }
  }

  delay(200);

Example 3: Software Interrupt

If you're committed to keeping this Qwiic then we can look for an interrupt by monitoring the Ambient Light Sensor directly rather than through a digital pin. In the code we'll use the light.readInterrupt() function call directly to see if there's been an interrupt issued. That's it!

language:c
void loop(){

  luxVal = light.readLight();
  Serial.print("Ambient Light Reading: ");
  Serial.print(luxVal);
  Serial.println(" Lux");  

  interrupt = light.readInterrupt();
  if (interrupt == 1)
    Serial.println("High threshold crossed!");
  else if (interrupt == 2){
    Serial.println("Low threshold crossed!");

  delay(200);

}

Example 4 - Power Save Mode

I won't break down this example code because you have all the necessary tools to get you started with the Ambient Light Sensor. However, if you plan on continuously reading ambient light data then give this sketch a try. It'll show you how to put the board into power save mode, which will save you battery life while still getting ambient light data. Check the Power Save Mode section under Hardware Overview as a reference when looking at the sketch.

Resources and Going Further

For more on the AS3935, check out the links below:

Need some other weather sensing parts for your project? Check out some of the ones listed below.

SparkFun Pressure Sensor Breakout - MS5803-14BA

SEN-12909
$80.50

Weather Meters

SEN-08942
Retired

SparkFun Weather Shield

DEV-13956
Retired

SparkFun Environmental Combo Breakout - CCS811/BME280 (Qwiic)

SEN-14348
Retired

Need some inspiration for your next project? Check out some of these related tutorials to sense your environment!

MAX30105 Particle and Pulse Ox Sensor Hookup Guide

The SparkFun MAX30105 Particle Sensor is a flexible and powerful sensor enabling sensing of distance, heart rate, particle detection, even the blinking of an eye. Get ready. Set. Shine!

Qwiic Ambient Light Sensor (VEML6030) Hookup Guide

The VEML6030 is a high accuracy ambient light sensor with 16-bit resolution. This I2C sensor can detect light similar to the human eye response. Start detecting light levels in your environment!

MicroMod Weather Carrier Board Hookup Guide

A quick guide to help to create your own MicroMod weather station using the MicroMod Weather Carrier Board and Processor of your choice.

Artemis Global Tracker Hookup Guide

The SparkFun Artemis Global Tracker combines the Artemis processor with an Iridium 9603N satellite transceiver, ZOE-M8Q GNSS transceiver, and MS8607 PHT sensor. With a clear view of the sky, this board allows you to send and receive short data messages from anywhere in the world including remote locations far beyond the reach of WiFi and GSM networks. Follow this guide to get started with the Artemis Global Tracker.