Papa Soundie Audio Player Hookup Guide

≡ Pages
Contributors: LightningHawk

Hardware Example Project: The Gag

I've been having too many "customers" coming through my office lately so I thought of creating a deterrent. The project senses when someone walks through my door and plays the quintessential convenient store bell. A counter keeps track of the number of customers and when it reaches 100 a cheering and clapping audio file is played and a bag holding balloons and confetti is untied by a servo motor releasing a party on the unsuspecting coworker.

Customer 100 gif

The Game Plan

For this project you will need the following the parts:

Hardware Hookup

The Fritzing diagram below provides the wiring for the project:

Fritzing Diagram

Having a hard time seeing the circuit? Click the image for a closer look.

Solder and wire the circuit together.

Final Assembly Image

When the PIR sensor detects movement, the Papa Soundie plays the respective audio file under the conditions set. When the 100th customer enters, pin 10 is sent HIGH. Pin 10 is attached to the Servo Trigger. The servo is used to pull the loose string which holds the bag holding the balloons and confetti closed. Here's a picture of the circuit mounted above the door.

Final Assembly hooked up above the door

It's not pretty but it works!

Example Sketch

Copy and paste the following code into the Arduino IDE. Hit upload, and see what happens! Make sure to select the correct board and COM port when uploading.

language:c
#include "SparkFun_PapaSoundie.h"

#define PIR_DOUT 9 

int count = 0;
int UNTIE = 10; //High signal to motor driver

PapaSoundie sfx = PapaSoundie();

void setup() {
  Serial.begin(115200);  // Serial is used to view Analog out
  // Analog and digital pins should both be set as inputs (not actually necessary for Analog):
  pinMode(PIR_DOUT, INPUT);
  pinMode(UNTIE, OUTPUT);
  Serial.println("Getting ready");
  sfx.begin();
}

void loop() {
  Serial.println(count);
  int motionStatus = digitalRead(PIR_DOUT);
  Serial.println("Looping");
  if (motionStatus == HIGH)
  {
    sfx.playFileNumber(1);
    motionStatus=LOW;
    delay(1000);
    count = count +1; 
    if (count == 100)
    {
      motionStatus = LOW;
      sfx.playFileNumber(2);
      digitalWrite(UNTIE, HIGH);
      delay(1000);
      sfx.playFileNumber(2);
      delay(1000);
      sfx.playFileNumber(2);
      delay(1000);
      count = 0;
      digitalWrite(UNTIE, LOW);
    }
  }
}

The Coup De Grace

This project was in no way a deterrent to keep people from entering my office; in fact, it was the opposite.

Balloons and confetti everywhere

What's worse, I was left with the mess. On second thought, this would make a great feature to any party.