Papa Soundie Audio Player Hookup Guide

≡ Pages
Contributors: LightningHawk

Audio Files

You can trigger up to 32 files from the SD card. With the extra space on the SD card you use much larger files than on the Little Soundie. For the Papa Soundie to keep track of the audio files they need to be named in a particular way; in a 7.3 format. Of the 7, the first five characters are reserved for the name of file and the last two characters are reserved for the file number. This is how the hardware knows which pin triggers which file. The .3 refers to the file extension, which can be either .ogg or .wav. For instance: file 1 could be AUDIO00.ogg or FILES00.wav. File 32 could be something like CLAPS31.ogg File one will be triggered when D2 is held high.

Quick Note about using WAV: The VS1000 developer library contains a simple WAV decoder, which is included in the firmware on the Papa Soundie. Currently the WAV decoder supports 8-bit ulaw, 8-bit linear PCM, and 16-bit linear PCM formats.

What is OGG Vorbis?

Ogg Vorbis is an audio file format developed by xiph, an open source multi-media company.

Ogg Vorbis is a fully open, non-proprietary, patent-and-royalty-free, general-purpose compressed audio format for mid to high quality (8kHz-48.0kHz, 16+ bit, polyphonic) audio and music at fixed and variable bitrates from 16 to 128 kbps/channel. This places Vorbis in the same competitive class as audio representations such as MPEG-4 (AAC), and similar to, but higher performance than MPEG-1/2 audio layer 3, MPEG-4 audio (TwinVQ), WMA and PAC.

Information courtesy of xiph.org

There are sites out there that will do the conversion for you without having to open a program, like this one.

Audacity is a great open source resource for all things audio that also has fantastic documentation.

There are several sound effects sites such Zapsplat and Soundbible to grab license free sound bites from and then convert to .OGG or .WAV using the methods listed above.

Binary Coded Playback

To get the most of your device and trigger more sounds than available pins the firmware is set up to trigger pins based on a binary code to associate an audio file with a specific set of pins. On the Papa Soundie you can trigger 32 files. Under the Binary column below the number represents which pins on the Arduino are pulled high and low from D6 to D2.

File No.Binary/IO Pin StateAudio File
100001AUDIO00.OGG
200010AUDIO01.OGG
300011AUDIO02.OGG
400100AUDIO03.OGG
500101AUDIO04.OGG
...
2811011AUDIO27.OGG
2911100AUDIO28.OGG
3011101AUDIO29.OGG
3111110AUDIO30.OGG
3211111AUDIO31.OGG

Note: One of our customers noticed that the files have to be numbered sequentially on the SD card. For example:
  1. AUDIO00.ogg
  2. AUDIO01.ogg
  3. AUDIO02.ogg
  4. You can't jump to AUDIO08.ogg, the next file has to be AUDIO03.ogg