Origami Paper Circuits

≡ Pages
Contributors: Sarah Al-Mutlaq

Finishing Touches

For the last step, you can solder wires to the copper tape.

Solder wires straight to the copper tape

Solder wires straight to the copper tape

Make sure if you are using the same color wires for both 5V and ground, as I did in the photo above, that you mark one of the wires so that you can tell them apart when you close up the flower.

Make sure that the 5V and ground copper wires never touch at any point. Since the copper wires are conductive on the surface, if they touch at any point, you will short your circuit and probably burn up your LED.

Once you have double checked your connections and made sure there aren't any shorts, connect your wire to ground and 5V. I have twisted mine to make them the stems of my flowers, or you could go further with magnets and metal sheets like my origami flower art installation and make something bigger.

Some of the LEDs I used were colored, and some where white. I suggest you try both out and see which color you like better, if using colored paper, or, if you just want to use white paper with a surprise color inside, that's fun too!

LIT Origami Kusudama Flower

And there you have it! Lovely light up flowers!

Bouquet of Flowers

Bouquet that is fun in the light...

Bouquet of Flowers in the Dark

..and in the dark!