Comments: MicroMod Teensy Processor Hookup Guide

≡ Pages

Looking for answers to technical questions?

We welcome your comments and suggestions below. However, if you are looking for solutions to technical questions please see our Technical Assistance page.

  • Member #488880 / about 4 years ago / 1

    The question as asked: " In general, how do I access the other 4 Serial Ports in Teensy MicroMod? "

    Which Teensy MicroMod pins have the other serial ports ?

  • Member #1709344 / about 4 years ago * / 1

    Confusion on MicroMod Teensy Serial:

    The MicroMod Teensy documentation says that it has seven serial ports. However, then later it describes only 3 ports.

    Micromod API    Micromod Pins    Teensy 4.0 Pins    Corresponding Teensy 4.0 Pins API   
    Serial1   (RX1: 19, TX1: 17)   (RX1: 0, TX1: 1)   Serial1
    Serial2   (RX1: 20, TX1: 22)   (RX4: 16, TX4: 17)   Serial4?

    Pins corresponding to Serial2 of Micromod Teensy are mapped to Pins corresponding to Serial4 of Teensy 4.0. So how do I access Serial communication on pins corresponding to Serial2 (RX2: 7, TX2: 8) of Teensy 4.0.

    In general, how do I access the other 4 Serial Ports in Teensy MicroMod?

  • Member #1719731 / about 5 years ago / 1

    RX2 is described as A2, but is listed as A3 in the pinout table.

  • Member #483997 / about 5 years ago / 1

    So this has everything the Teensy 4.1 has broken out except the no native Ethernet?

  • brtaylor / about 5 years ago / 1

    More discrepancies, COPI is labeled as Pin 59 here and in the schematic GOTO flag, but the pin label in the schematic is SPI_SDO (i.e. the opposite of COPI). Similar discrepancy in the schematic Pin 61 (CIPO).

  • brtaylor / about 5 years ago / 1

    There's a discrepancy between the schematic (https://cdn.sparkfun.com/assets/0/c/7/a/f/MicroMod_Teensy_ProcessorBoard_Schematic.pdf) and the table in this guide. The table here shows USB_D+ as Pin 5 and USB_D- as Pin 3. USB_HOST_D+ as Pin 37 and USB_HOST_D- as Pin 35. The MICROMOD-2222 connector in the schematic shows USB_D+ as Pin 3 and USB_D- as Pin 5. USB_HOST_D+ as Pin 35 and USB_D- as Pin 37.

    • El Duderino / about 5 years ago / 1

      Thanks for pointing those swapped signals out. The table is fixed now.

  • Defragster / about 5 years ago / 1

    Update Pending? This guide shows 8MB flash ... instead of 16MB

    • El Duderino / about 5 years ago / 1

      That has been updated. Minor typo from our other Teensy tutorial. The Teensy MM has 16MB Flash.


If you've found an issue with this tutorial content, please send us your feedback!