Measuring Internal Resistance of Batteries

≡ Pages
Contributors: Shawn Hymel

Internal Resistance

When designing a circuit with a battery, we often assume that the battery is an ideal voltage source. This means that no matter how much or little load we attach to the battery, the voltage at the source's terminals will always stay the same.

Battery as ideal voltage source

If we model this battery as an ideal voltage source, changing the value of RL does not affect the voltage between the battery's terminals

In reality, several factors can limit a battery's ability to act as an ideal voltage source. Battery size, chemical properties, age, and temperature all affect the amount of current a battery is able to source. As a result, we can create a better model of a battery with an ideal voltage source and a resistor in series.

Battery as ideal voltage source and inline resistor

Batteries can be modeled as an ideal voltage source with a series resistor (labeled RI)

We can measure the voltage of a battery across its terminals without any load connected. This is known as the open-circuit voltage (VOC).

Voltage of a AA

Measuring the voltage of a AA alkaline cell with no load attached

Note that because no current is flowing across the internal resistor, the voltage drop across it is 0 V. Therefore, we can assume that VOC is equal to the voltage of the ideal voltage source in the battery.

Open circuit voltage

If we connect a load across the battery, the voltage across the terminals drops.

Voltage of a loaded AA

In this, we are measuring the voltage drop across a 4 Ω resistor

This drop in voltage is caused by the internal resistance of the battery. We can calculate the internal resistance if we take readings of the open-circuit voltage and the voltage across the battery's terminals with a load attached.

To start, we create a diagram showing our circuit.

Loaded voltage

Here is our circuit. We want to calculate RI.

We can plug in the loaded voltage we measured (VL) and the value of the resistor (RL) into Ohm's Law to get the current flowing through the circuit (I).

alt text

alt text

alt text

alt text

alt text

We also need to get the voltage across the internal resistor. We can do that using Kirchhoff's Voltage Law. Simplified for this circuit, we can say that the voltage drop across both resistors must add up to the voltage of the ideal voltage source.

alt text

alt text

alt text

Now that we know the voltage drop across the internal resistor and the current through it, we can use Ohm's Law again to find its resistance.

alt text

alt text

alt text

From this, we can see that the internal resistance (at this moment) of the AA cell is 0.273 Ω.

NOTE: We can only take a snapshot of the internal resistance with this method. The internal resistance can vary with things like battery age and temperature. In 10 minutes, the resistance value might be different! A common AA alkaline battery might have anywhere between 0.1 Ω and 0.9 Ω internal resistance.