Light-Up Valentine Cards

≡ Pages
Contributors: Gella

Step 6: Prepare Pop Up

Time to cut out our pop up pieces. Click the links below to visit the pop up card's website for full instructions on assembling.

I <3 U Instructions

Note: Glue a piece of vellum or parchment paper to the back of the heart outline before you fold the pop up to make it easier to attach.

The original project is in Korean, so we've included a tutorial we found a video on youtube showing you the process.

Pixel Heart Instructions

Note: This card can be tricky to pop up since there are so many small cuts. We've found using a pencil or thin marker to pull up the folds one at a time from the bottom of the heart up to the top makes it a little easier.

Frame Instructions

Note: Follow the folding instructions from the Window card in our Christmas Pop Up card tutorial. Use a piece of parchment paper or vellum behind the frame to create a base to attach stickers or cut outs, or draw on with markers. We chose a pet lovers theme, but feel free to create your own unique scene.

alt text