Keyboard Shortcut, Qwiic Keypad

≡ Pages
Contributors: santaimpersonator

Introduction

You may not realize it, but you probably often use keyboard shortcuts for common tasks that, otherwise, were previously extremely monotonous. A perfect example of these shortcuts are the Cut, Copy, and Paste commands, which are almost universally used in every computer application today. Originally, people used to cut (with special scissors) and paste these changes manually.

In this guide, we will cover how to utilize the RedBoard Turbo to emulate an HID keyboard that responds to inputs from the Qwiic Keypad to create your own custom shortcut keypad. This is perfect for gaming hotkeys, keyboard shortcuts that require more than two button combinations, or for command line/data/text entries.

Hotkey Keypad

This will be similar to the Enginursday Blog Post: Pressing Our Buttons, but without the complex soldering. Although not necessary, it would be good to review the blog post.

Please be aware that the example code below is written to run explicitly on Windows OS. For Mac OS, you will need to modify the code for the appropriate Mac OS keycodes.

Required Materials

For this project, you will need the following products. You may already have a few of these items, so feel free to modify your cart based on your needs.

SparkFun RedBoard Turbo - SAMD21 Development Board

DEV-14812
$22.50 $11.95

SparkFun Qwiic Keypad - 12 Button

COM-15290
$13.50

Qwiic Cable - 100mm

PRT-14427
Retired

Suggested Reading

If you haven't already gone through the hookup guides for each of these parts, we highly suggest starting off there to understand the basic functionality of each board:

Qwiic Keypad Hookup Guide

If you are tired of taking up GPIO pins, wiring a bunch of pull up resistors, and using firmware that scans the keys taking up valuable processing time... check out the new Qwiic Keypad.

RedBoard Turbo Hookup Guide

An introduction to the RedBoard Turbo. Level up your Arduino-skills with the powerful SAMD21 ARM Cortex M0+ processor!

Qwiic Connect System

This project utilizes the Qwiic connect system. We recommend familiarizing yourself with the Logic Levels and I2C tutorials (above) before using it. Click on the banner above to learn more about our Qwiic products.

For a better understanding of how example codes work, please review the following references for the platform you are interested in: