Installing a Bootloader on the MicroView

≡ Pages
Contributors: jimblom

Gathering the Tools

Before you get going, there are a few tools you'll need to gather: something to pry open the MicroView, a method for connecting to the small vias, and an AVR programmer. There are many options for each of those tools, we'll list a few in the sections below.

For those short on one tool or another, we've created the MicroView Bootloading Kit, which includes everything you'll need to follow along with this tutorial.

MicroView Bootloading Kit

The kit is an especially great deal if you need an AVR programmer -- the price for the kit (which includes a knife, jumpers, and resistors) is the same as the programmer itself.

An Opener

A thin, flat, rigid-ish tool is required to separate the MicroView's shell from the lens covering it. This can be a spudger, hobby knife, or a thin flathead screwdriver (the smallest bit in our Pocket Screwdriver works).

Pocket Screwdriver Set

TOL-12891
$5.50

Hobby Knife

TOL-09200
$3.75

The knife has a lower potential for scratching your MicroView's shell, but the tip will also probably break on your first pry attempt. Use a more veteran, dulled blade if you can. Or, better yet, sacrifice a blade and break the sharp end of the tip off.

A Programmer

There are a multitude of tools that can perform the task of reprogramming a MicroView over ISP. There are boards built for the task, like the Tiny AVR Programmer, STK500 USB Programmer, or the AVR Pocket Programmer.

STK500 Compatible USB Programmer

PGM-08702
Retired

Pocket AVR Programmer

PGM-09825
Retired

Tiny AVR Programmer

PGM-11801
Retired

Even if you don't have a dedicated AVR programmer, you might have a programmer and not even know it! Most Arduino's can be programmed to replicate an AVR Programmer. If you have an Arduino Uno, RedBoard, Pro, or, really, any ATmega328P-based Arduino, you're already good-to-go.

Arduino Uno - R3

DEV-11021
$27.60

Arduino Pro 328 - 5V/16MHz

DEV-10915
Retired

SparkFun RedBoard - Programmed with Arduino

DEV-12757
Retired

By loading the ArduinoISP sketch onto your Arduino, it'll transform into a USB AVR programmer. Arduinos programming Arduinos: madness!

Jumper Wires

To connect between your Programmer and the MicroView, you'll need six, individual male-to-male jumper wires. Most M/M jumpers will do, including the standard or premium sets.

Hook-Up Wire - Assortment (Solid Core, 22 AWG)

PRT-11367
$25.95

Jumper Wires Standard 7" M/M - 30 AWG (30 Pack)

PRT-11026
$3.50

Jumper Wires Premium 6" M/M Pack of 10

PRT-08431
$5.25

You can even use solid-core wire if you'd like.

The Arduino IDE

There are a handful of software tools that can be used to reprogram AVRs. The easiest program, and the one we recommend, is the good ol' Arduino IDE. Arduino has a built-in tool, which allows you to burn a bootloader into any of its many boards, it makes programming a bootloader as easy as two clicks.

Burn bootlaoder in Arduino

(Optional, Recommended) Solder Tools or Thin-Gauge PTH Resistors

The hardest part of this whole process is connecting your programmer to three of the MicroView's tiny ISP pins. Due to space restrictions they're broken out to a trio of small, exposed vias.

MV exposed vias

After lifting the cover off your MicroView, you'll need to connect to those vias labeled "11", "12", and "13".

If you apply enough steady pressure, you can complete those three connections without soldering or connecting anything else. Be warned, though, that it'll take a few tries to get right; if you're low on patience, frustration might brew.

If you'd like to avoid soldering to your MicroView, one trick is to plug through-hole, 0Ω (or, at least, very low resistance) resistors into the MicroView's three ISP vias. The trick is finding resistors with thin enough leads. The 0Ω resistors on our Resistor Kit work perfectly for this task, but watch out, many other resistors -- especially those rated for ¼W and above -- have too-thick leads.

(There are all sorts of other, clever ways to connect into those vias. For example, you can poke them with sewing needles. You just need something with a diameter under about 0.015" that conducts electricity.)

Instead of jamming resistors into the vias, if you have soldering tools handy, you can make the programming process a lot smoother by temporarily soldering a jumper wire to the test pin -- creating a reliable electrical connection between MicroView and programmer. A simple iron, and some solder is all you should need.


Solder Lead Free - 15-gram Tube

TOL-09163
$4.95

Soldering Iron - 30W (US, 110V)

TOL-09507
$11.50

Solder Wick #2 Yellow - No Clean

TOL-09327
$2.95

Soldering Iron - 30W (EU, 230VAC)

TOL-11650
Retired

Solder wick might help when you get to disconnecting the wires and cleaning up.