Installing a Bootloader on the MicroView

≡ Pages
Contributors: jimblom

(Carefully) Opening the Case

The AVR ISP programming interface requires six pins: VCC, GND, RST, MOSI, MISO, and SCK. VCC (power), GND (ground), and RST (reset) are all broken somewhere along the MicroView's readily available pair of 8-pin headers. Unfortunately, the three SPI signals are not broken out to the headers, they're tucked away, inside the enclosure, broken out to three unmasked vias. To expose these pins, you'll have to remove the Microview's covering lens and lift the display up.

Grab your spudger, hobby knife or small, flathead screwdriver. And find a flat, steady surface to do the deed.

The opener and the MicroView

If you're using a sharp-edged hobby knife, you may want to grab a pair of pliers and snap off a small chunk of the tip to get a more blunt, flat edge.

Knife edge snapped blunt

The lens cover is held in place by two securing notches on the left and right sides of the enclosure. Try to expose as much of a gap on one side as you can, by sliding the lens to either the left or right. You may be able to see one of the securing notches.

MV retaining notch

Insert your opener somewhere between that notch and the bottom of the cover. You should be able to push it in about 2mm, before a beveled edge inside the enclosure gets in the way. Be gentle, but try to push in as far as you can to get more leverage.

Inserting the knife

Then pry up the cover by tilting the opener towards the outside of the MicroView.

Prying the top off

Once the edge of the screen has popped off, grab it with your fingers and pull it off.

Cover removed

The exposed pins for MISO, MOSI, and SCK are just under the display. To access them, very carefully pry the OLED up. The OLED is connected to the PCB via a thin, black connector; it's fragile, take great care not to place any extra stress on it.

Display lifted off PCB

Those three, small unmasked vias, labeled "11", "12", and "13", are what we're after!