Flashlight Kit

≡ Pages
Contributors: M-Short

Introduction

The Flashlight Soldering Kit is a basic soldering kit designed to help teach the basics of through hole soldering and circuit design. This tutorial will go over the basics of a circuit, how to solder, and show you how to build your own flashlight.

SparkFun Basic Flashlight Soldering Kit

KIT-14877
$5.50

Required Tools

To build this you will need a few basic tools such as a soldering iron, solder, and snippers. You should also maintain good ventilation and eye protection as well!

Soldering Iron - 60W (Adjustable Temperature)

TOL-14456
$25.95

Solder Lead Free - 15-gram Tube

TOL-09163
$4.95

Diagonal Cutters

TOL-08794
$3.75

SparkFun Safety Glasses

SWG-11046
$5.10

Suggested Reading

Here are a few basic tutorials on some of the concepts that we will cover. There are also links throughout the tutorial to give you more information on a topic if you are confused or just interested in learning more.

How to Solder: Through-Hole Soldering

This tutorial covers everything you need to know about through-hole soldering.

Resistors

A tutorial on all things resistors. What is a resistor, how do they behave in parallel/series, decoding the resistor color codes, and resistor applications.

Light-Emitting Diodes (LEDs)

Learn the basics about LEDs as well as some more advanced topics to help you calculate requirements for projects containing many LEDs.

Polarity

An introduction to polarity in electronic components. Discover what polarity is, which parts have it, and how to identify it.

Hardware Overview

Contents

Inside your kit you'll find a few parts. There should be a PCB, a small coin cell battery, a battery holder, an LED, a resistor, and a switch. We'll get into what each of these components looks like and what they do in the next section. Missing any parts? Sometimes one of those tiny little components can get misplaced. If you're missing any parts contact our customer service team, and we'll get you those missing parts in a jiffy.

Picture of all components in the kit

Before we get started lets take a basic look at the PCB. On the front you can see markings and outlines for the 4 different components as well as some labels. You can also see the traces on the board and how they go from one component to another making a complete circle. On the back you see that the holes have a copper ring around them so you can solder them. You'll also see a schematic of the circuit showing all 4 components (with each labeled). We'll get into what each component does in a minute.

Front of PCB Back of PCB
Front of the Board Back of the Board

Flashlight Circuit

The Circuit

So, what does our circuit do? A completed circuit is a path where electrons can flow. Consider the battery our source of electrons. Current is how we measure the flow of those electrons. Starting with the positive end of the battery, you can see the path it takes along the left side of our PCB up to the resistor. Batteries are basically our power house that stores power and outputs that power in terms of current (how fast the electrons are moving) and the voltage (the amount of pressure pushing those electrons through the circuit).

Photo of battery holder Battery symbol
Battery Holder Schematic Notation for Battery

The Resistor

The resistor is like a tube that restricts the amount of current that can get through. This resistor minimizes the current that gets to your LED so we don't give the LED too much current and destroy it. If you are curious how this works you can check out our LED tutorial to see how to properly size a resistor. If you look closely at your resistor you'll notice some color bands. In this kit we use a 5 band resistor (brown, black, black, gold, brown); this is a 10 Ohm resistor with a 1% tolerance. Resistors are not directional, meaning they can be used in the circuit in either a forwards configuration (brown, black, black, gold, brown) or a backwards configuration (brown, gold, black, black, brown) and still function correctly.

Photo of Resistors Resistor symbol
Resistor Schematic Notation for Resistor

The LED

Next we have the LED. LED stands for light emitting diode. A diode is 2 pieces of semiconductor placed together to allow current to only flow in one direction. This is one of the reasons your LED is polarized (meaning it matters which way you hook it up). The current can only flow from the positive side (anode) to the negative side (cathode). In this case we are using a light emitting diode, which does exactly what it sounds like. It is a diode that emits light which is very convenient for a flashlight. Using different substances in the diode allow for different colors; for our flashlight we chose a white LED.

Photo of LED LED symbol with Anode and Cathode labeled
LED Schematic Notation for LED

The Switch

Last we have our switch. A switch is actually a mechanical part, meaning you have to physically move the switch Physically moving the switch will connect the negative pin from your LED to the negative pin of your battery, thus completing the circuit. Flip the switch the other way and the switch physically disconnects those 2 components.

Photo of Switch Switch symbol
Switch Schematic Notation for Switch

The Schematic

Once you put everything together, our electrons will flow (when the switch is in the On position) and our flashlight will turn on. Here is a picture of the completed board and the full schematic (also found on the back of the PCB).

Photo of Assembled Kit Schematic of Flashlight Kit
Completed Flashlight Schematic Notation for Completed Circuit

How to Solder

Soldering is basically melting metal. Solder is a specially formulated metal with a relatively low melting point. For example the melting point of solder is typically about 370F(188C) to 428F(220C) where as the melting point of copper is 1984 F (1085C). With a soldering iron we can melt the solder in order to connect two pieces of metal. This connection is both mechanical (physically holds the parts together) and electrical (allows electricity to flow between them). If you look at the front of your PCB, you'll can see the copper traces that are run just under the surface and are exposed in the holes we are going to solder to.

A Tip About Tips

So, how do you solder? The goal is to heat the metal pads and the components and then let them melt the solder. Do not try to melt the solder and then wipe it where you want it as that will both cause bad joints and get pretty messy. Soldering irons come with many different tips. While finer points may work better for finer work, fatter tips hold heat better and therefore can be used more quickly and efficiently than finer points. Ultimately it is a personal choice, but the tip your iron comes with is a good place to start.

Position is Everything

When soldering you'll want to avoid trying to heat things with the point of the iron. Use the side near the tip for the most effective heat transfer. Place the iron next to the joint between the board and the component, wait about 1 second and then feed about 1/2in (about 1cm) of solder into the joint. It should melt immediately and make a nice shiny mountain of solder. Once you have enough solder remove the solder and then the iron. If you remove the iron first your roll of solder will be stuck to your joint. If this happens don't worry, just heat up the joint, remove the solder (and then the iron) and you are good to go. If it doesn't melt right away you may need to wait a bit longer, check your iron placement, clean your tip, or increase the temperature of your iron.

Check out the Vimeo version here.

Keep it Clean

Don't forget to clean your tip periodically! I usually try to do this every time I put the iron back in the stand. No matter what you do you, you are likely to end up with burnt on gunk on the end of your iron. A lot of that will be flux (a substance used to make the solder flow better that is actually part of a lot of solders you buy), or old burnt solder. Most soldering iron stands will have a spot for a sponge to wipe your tip on. You will need to use either a brass sponge or a regular sponge that is wet to wipe off your tip. For more soldering tips and info check out our soldering tutorial.

Graphic on soldering best practices

Click for a larger image.

Assembly Guide

We are going to start with the smallest components first and add parts in as they get larger. This makes it easier to get your components to stay put when you are soldering them in.

Attaching the Resistor

First we'll add the resistor. Bend the ends down at a right angle so that it looks like a 'U'. Personally I like to just bend them over my finger, but depending on your finger size this may or may not work well. We are then going to insert each end into the board in the spot labeled "Resistor". Turn the board over and pull the leads through. Your resistor should be sitting pretty flush to the PCB. It doesn't have to be perfect, but the closer it is, the neater it will look. Now you can go ahead and bend the legs over a bit to help hold everything in place. Then solder the 2 joints (see above for correct solder methods).

Photo of resistor being bent over Photo of resistor being soldered to the board
Shaping the Resistor Solder Points for Resistor Legs

Attaching the Battery Holder

Next we are going to solder on the battery holder. Make sure you put it in the right way! The board will have an outline on it showing which way it goes. Solder the 2 pins on the bottom side of the board. The battery holder should be fairly flush to the board. While it doesn't need to be perfectly flush, it needs to be flush enough that both feet go through the board and can be soldered. If you solder in the first pin and find that it isn't sitting flush don't worry. Put pressure on the board with one hand and heat up the joint with the other hand. Once the solder melts the part should snap into place.

Attaching the Switch

Next is the switch. Insert the switch (either direction is fine) and flip the board over Solder the 3 switch pins into place. Again the switch should be fairly flush to the board. Look at that, you are becoming a pro at this!

Photo of switch and battery holder in board Photo of switch and battery holder soldered
Switch Placement on the Front of the Board Solder Points for the Switch on the Back of the Board

Attaching the LED

The final solder step is the LED. LEDs are polarized, meaning the direction you insert the LED matters. If you take a look at your LED you'll notice one leg is longer than the other. Insert the LED with the long leg on the side labeled "Long Leg". Insert the LED almost to the board and bend it over so it lays in the slot on the top of the PCB. It doesn't have to be exact, but this will allow your flashlight to shine forward instead of straight up and in your eyes. Then you can bend the legs back on the back of the PCB to help hold it in place and solder the legs.

Photo of LED showing one leg longer than the other Photo of LED being folded over on board
LED - Note One Leg is Longer! Placement and Shaping of LED

Clean Up

Next is a bit of clean up. Clip off all your extra leads on the back side of the board; you don't want things making connections they shouldn't and the switch pins can poke you if you are not careful. Get a good pair of cutters and snip those leads off! The last step is to put your battery in, make sure the switch is in the "On" position, and let your light shine!

Photo of resistor being bent over Photo of resistor being bent over
Front of the Finished Board Back of the Finished Board

Troubleshooting

Flashlight Not Turning On

  • Make sure you turned the switch to the On position
  • Make sure you inserted a new CR2032 battery (and that it is in + side up)
  • Double check all solder joints to make sure they have a good connection
  • Make sure you soldered your LED in the correct way
  • Make sure you clipped your leads so you don't have any shorts

Flashlight Flickering

  • Make sure all components are soldered in place well
  • Make sure battery is in securely
  • Make sure switch is pushed all the way up
  • Make sure there are no "extra" connections - the leads on the back side of the board should be cleanly clipped.

Flashlight Is Dim

  • Make sure resistor value is 10Ω (brown-black-black-gold-brown)
  • Replace battery as needed

Resources and Going Further

Now that your flashlight is lighting everything up, where do you go from here? Check out some of our different tools as well as some additional kits you can solder together. Also, check out some of our other soldering tutorials, or just start building your own projects.

Resources for This Kit:

For more information, check out the resources below:

Soldering Kits

SparkFun Simon Says - Through-Hole Soldering Kit

KIT-10547
$29.95

SparkFun WeevilEye - Beginner Soldering Kit

KIT-10723
$9.95

SparkFun Learn to Solder - Simon Says

KIT-13708
$54.95

SparkFun Binary Blaster Kit

KIT-12037
$32.95

Airplane Soldering Kit - White & Red

KIT-29526
$19.95

Mini Airplane Soldering Kit - Red

KIT-29525
$14.95

Mini Rocket Soldering Kit - Red

KIT-29589
$19.95

Bicycle Soldering Kit

KIT-29527
$15.95

Soldering Tools and Kits

PINECIL Soldering Iron Kit

KIT-24063
$119.95

Magnetic Third-Hand Kit

TOL-19944
$81.50

Soldering Iron - 60W (Adjustable Temperature)

TOL-14456
$25.95

Insulated Silicone Soldering Mat

TOL-14672
$15.95

Solder Lead Free - 15-gram Tube

TOL-09163
$4.95

Solder Tip Tinner and Cleaner

TOL-13246
$11.50

SparkFun Safety Glasses

SWG-11046
$5.10

Hakko Solder Reel

TOL-30646
$14.95

More Tutorials

Looking for more of a challenge? Try soldering the same circuit together without using a PCB like the 3D Printed Illuminated Wand Prop, learn how to work with RGB LED Strips, and more!

Electronics Assembly

How SparkFun assembles SMD electronics.

Let It Glow Holiday Cards

Craft a glowing card for friends and family this holiday season with paper circuits - no soldering required!

Non-Addressable RGB LED Strip Hookup Guide

Add color to your projects with non-addressable LED strips! These are perfect if you want to control and power the entire strip with one color for your props, car, fish tank, room, wall, or perhaps under cabinet lighting in your home.

3D Printed Illuminated Wand Prop

In this tutorial, we will learn about how to create a theatrical prop for a performance by 3D printing a wand and adding an LED.

Looking for more soldering tutorials? Check out some of these related tutorials:

Large Solderable Breadboard Hookup Guide

This breadboard has a couple of tricks up it's sleeve!

How to Solder: Castellated Mounting Holes

Tutorial showing how to solder castellated holes (or castellations). This might come in handy if you need to solder a module or PCB to another PCB. These castellations are becoming popular with integrated WiFi and Bluetooth modules.

How to Use a Hot Air Rework Station

Hot-air stations or heat guns are very useful tools and are essential for any electronics workbench. When working with or building printed circuit boards, there is a lot of room for errors to be made. Have no fear though, there are ways to remedy this with a hot air rework station!

How to Work with Jumper Pads and PCB Traces

Handling PCB jumper pads and traces is an essential skill. Learn how to cut a PCB trace, add a solder jumper between pads to reroute connections, and repair a trace with the green wire method if a trace is damaged.