BadgerHack: Sensor Add-On Kit

Pages
Contributors: Sarah Al-Mutlaq

Code

Analog sensors work by providing a voltage output that is proportional to the what they are measuring. This means with something like analog temp sensor we are using, the output voltage can be converted to temperature easily using the scale factor of 10 mV/°C. However, a little bit of math is required depending on what the input voltage is, so that will change based on if you are using the Badgerstick at 3.3V or the Redstick at 5V. (But don't worry, this has already been done for you in the code.)

The soil moisture sensor works the same way, but we are leaving the data as is, since converting it to something usable like kg of water per kg or soil would be very difficult without knowing what kind of soil you have and how it reacts to electricity.

Plug the USB side of your BadgerStick into your computer. Make sure "BadgerStick" and the associated COM port are selected in the Arduino IDE, and click upload.

If you have the Redstick Make sure "Arduino Uno" and the associated COM port are selected before uploading. Also if you are using a Redstick, you will need to go into the code and change one variable at the end to have the correct temp output (instructions in the code).

language:c
/**
 * BadgerHack Sensor add on kit
 * Sarah Al-Mutlaq @ SparkFun Electronics
 * January 22, 2016
 * 
 * Scrolls temp reading and soil moisture across the Badger's LED array.
 * 
 * License: http://opensource.org/licenses/MIT
 * 
 * THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR
 * IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY,
 * FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN NO EVENT SHALL THE
 * AUTHORS OR COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER
 * LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING FROM,
 * OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS IN
 * THE SOFTWARE.
 *
 *NOTE: for this add on kit, you will want to power the badger
 *through its USB port, so that you know you have 3.3V instead 
 *of an unknown amount from a battery pack, which would make 
 *the temperature reading less accurate. 
 */

#include <SparkFun_LED_8x7.h>
#include <Chaplex.h>



// Global variables
static byte led_pins[] = {2, 3, 4, 5, 6, 7, 8, 9}; // Pins for LEDs
const int moisturePin = A0;     //signal pin from the moisture sensor
                                //is hooked up to pin A0 on the badger
const int temperaturePin = A4;  //singnal pin from temp sensor is 
                                //hooked up to pin A4 of the badger        

void setup() {

  // Initialize LED array
  Plex.init(led_pins);

  // Clear display
  Plex.clear();
  Plex.display();
}

void loop() {

  float voltage;

  // First we'll measure the voltage at the temperature analog pin. Normally
  // we'd use analogRead(), which returns a number from 0 to 1023.
  // Here we've written a function (further down) called
  // getVoltage() that returns the true voltage (0 to 5 Volts)
  // present on an analog input pin.

  voltage = getVoltage(temperaturePin);

  // Now we'll convert the voltage to degrees Celsius.
  // This formula comes from the temperature sensor datasheet:
  float tempC = (voltage - 0.5) * 100.0;
   // While we're at it, let's convert degrees Celsius to Fahrenheit.
  // This is the classic C to F conversion formula:
  float tempF = tempC * (9.0/5.0) + 32.0;
  char temperature[10];
  char str_tempC[6];
  char str_tempF[6];

  //This converts the floating variable of temperature to a 
  //sting so that we can print that on the array:

  /* 4 is mininum width, 2 is precision; float value is copied onto str_temp*/
  dtostrf(tempF, 4, 2, str_tempF);
  sprintf(temperature,"Temp: %s F", str_tempF);

  //dtostrf(tempC, 4, 2, str_tempC);               //Uncomment these lines and
  //sprintf(temperature,"Temp: %s C", str_tempC);  //comment the previous lines 
                                                   //If you want to see temp in C

  //This prints the string we just made to the badger array:
  Plex.scrollText(temperature, 1);

  //wait for 7 secounds while scrolling temp:
  delay(7000); 

  //Read the value of the moisture sensor and print that directly 
  //to the badger array:

  int sensorValue = analogRead(moisturePin);
  char moisture[20];

  sprintf(moisture, "Moisture level: %i", sensorValue);

  Plex.scrollText(moisture, 1);

  //wait for 11 seconds while scrolling moisture level:
  delay(11000); 

  // Stop scrolling the text
  Plex.stopScrolling();
  delay(2000);
}

float getVoltage(int pin)
{
  // This function has one input parameter, the analog pin number
  // to read. You might notice that this function does not have
  // "void" in front of it; this is because it returns a floating-
  // point value, which is the true voltage on that pin (0 to 5V).

  // You can write your own functions that take in parameters
  // and return values. Here's how:

    // To take in parameters, put their type and name in the
    // parenthesis after the function name (see above). You can
    // have multiple parameters, separated with commas.

    // To return a value, put the type BEFORE the function name
    // (see "float", above), and use a return() statement in your code
    // to actually return the value (see below).

    // If you don't need to get any parameters, you can just put
    // "()" after the function name.

    // If you don't need to return a value, just write "void" before
    // the function name.

  // Here's the return statement for this function. We're doing
  // all the math we need to do within this statement:


  return ((analogRead(pin) * 0.0048875855327468) * (3.3/5));

  // This equation converts the 0 to 1023 value that analogRead()
  // returns, into a 0.0 to 3.3 value that is the true voltage
  // being read at that pin.
  //If you are using a 5V device just erase the "*(3.3/5)" in
  //the above equation.
}