BadgerHack: Gaming Add-On Kit

≡ Pages
Contributors: Shawn Hymel

Hardware Hookup

To begin, snap off 15 pins from the break-away headers, and solder them to the through-holes on the side opposite the LED array of the BadgerStick.

Solder pins to the BadgerStick

Solder the Thumb Joystick to the Thumb Joystick Breakout board.

Solder joystick to breakout board

Snap off 5 pins from the break-away headers, and solder them to the through-holes on the Joystick Breakout Board.

Solder pins to joystick breakout board

Connections

Place the BadgerStick in the breadboard with pin 10 in position i13 and pin 5V in position i27.

Connect the rest of the components as follows:

Component Breadboard
Thumb Joystick Breakout* i7 (VCC) i6 (VERT) i5 (HOR) i3 (GND)
Pushbutton c20 c22 f20 f22
Pushbutton c28 c30 f28 f30
Jumper Wire ( - ) g30
Jumper Wire ( - ) g25
Jumper Wire ( - ) g22
Jumper Wire ( - ) j3
Jumper Wire j7 g23
Jumper Wire j6 g18
Jumper Wire j5 g17
Jumper Wire g21 g28

* Pins not listed are not used.

Gaming Badger Fritzing diagram

Wire colors correspond to the colors of the table above.

IMPORTANT: You can leave the battery pack soldered into the BadgerStick if you desire. If you remove the battery pack, you will need to supply power through another means, such as a USB port or a USB extension cable.

You should now have a makeshift game controller with a tiny LED screen!

Gaming badger with batteries