ATX Power Connector (4-Pin) Breakout Hookup Guide

≡ Pages
Contributors: bboyho

Power Supply Options

Below are options where you will encounter the 4-pin connector.

ATX Power Supply

ATX power supplies usually have a number of power connectors available to power components for a desktop computer. The connector of interest in the image below is the second connector from the right. This 4-pin power connector is intended to power 12V and 5V computer peripherals (such as disk drives). Depending on the manufacturer of the power supply, the quantity of each connector can vary. If you want to grab some juice for your project from this type of power supply, you'll need to connect the breakout board to this port.

ATX power supply with power connectors

Image Courtesy of User "Smial" on Wikipedia

12V/5V (2A) Power Supply

Certain wall adapters also take advantage of this standard 4-pin port like the 12V/5V (2A) power supply in the catalog. If your project requires either/both 12V and 5V for power you can also connect the breakout board to this power supply.

4-Pin ATX Connector and Wires Inserted to Breakout Board