Addressable LED Strip Hookup Guide
Contributors:
Nick Poole
Resources and Going Further
Now go forth and add lights to everything! It's worth noting that the RedStick is powerful enough to address a lot more than 60 LEDs, but you'll need to beef up the power supply before you start chaining strips together.
Need more LEDs? Check out these other form factors of the WS2812 Addressable LED strips:
Check out our selection of power supplies, if you need to power more LEDs:
Retired
Retired
Retired
Retired
Did you cut the strip? Check out the LED Strip pigtail connector to easily connect the cut strips:
For more blinky fun, check out these other great SparkFun tutorials:
Sound Detector Hookup Guide
The Sound Detector is a microphone with a binary output. This guide explains how it works and how you can use it in your projects.
SX1509 I/O Expander Breakout Hookup Guide
Learn how you can use the SX1509 to control 16 LEDs or up to 64 buttons with just two pins.
AVR-Based Serial Enabled LCDs Hookup Guide
The AVR-based Qwiic Serial Enabled LCDs are a simple and cost effective solution to include in your project. These screens are based on the HD44780 controller, and include ATmega328P with an Arduino compatible bootloader. They accept control commands via Serial, SPI and I2C (via PTH headers or Qwiic connector). In this tutorial, we will show examples of a simple setup and go through each communication option.
Light Up Your 3D Printer's Bed
Having issues viewing your print in a dark lit room? In this tutorial, we will be using LED strips to light up a print bed's area on a LulzBot 3D printer!