Addressable LED Neon Flex Rope Hookup Guide

≡ Pages
Contributors: bboyho

Hardware Hookup w/ Power Only

When powering the LED neon flex rope with only power, it will display a demo. Insert the 3-prong power cable into the 24V power supply. Then make the following connections with using a female DC barrel jack adapter.

24V Power Supply Female DC Barrel Jack Adapter LED Neon Flex Rope Pinout
Center Positive + Vcc (Red Striped) = 24V
Clear (Middle) = DAT
GND - Clear (Side) = GND

Once connected, insert and fasten the adapter to the female bare wire connector into the LED neon flex rope. The setup should look like the image below. Tape was used to insulate the DAT pin since the wire was exposed.

Hardware Hookup with Only Power