RFID Basics

≡ Pages
Contributors: Nate, Toni_K, a_cavis

RFID Frequencies

As well as active and passive systems, RFID systems can also be broken out into different frequencies.

Some frequencies and systems are designed to only read one tag at a time, while others can read multiple. Cost of readers can also vary wildly based the frequency rating of the modules. In prior years a reader capable of reading multiple tags was in the thousands of dollars, sometimes tens of thousands. These systems were unattainable for most hobbyists and prototypers. However, this is finally beginning to change, and multi-read capable readers are becoming much more affordable.

Check out the following chart for a basic break down of the frequencies, and their associated properties.

A Few Common RFID Reader Types
Frequency AKA Range Read/Write Read Multiple Tags Simultaneously Average Tag Cost
Low Frequency (120-150 kHz) "Chips/microchips" (in veterinary applications), prox cards, HID cards (both trade names) Up to 20 cm/ < 1 foot Read Only No $0.50
High Frequency (13.56 MHz) MiFare, NFC Up to 1 meter Read/write No $1
Ultra High Frequency (433 MHz, 860-920 MHz) Long-range RFID, powered RFID Up to 100 meters Read/write Yes $0.05
Information from Wikipedia: Radio-frequency identification