RETIRED 2 - BadgerHack

This Tutorial is Retired!

This tutorial covers concepts or technologies that are no longer current. It's still here for you to read and enjoy, but may not be as useful as our newest tutorials.

Pages
Contributors: Shawn Hymel

Make a Game

OK, so the display might be small (don't get your hopes up of running Doom on an 8x7 monochrome display). However, we can use it to display information and even play some basic games.

Remember the game Breakout? I don't, really, but the concept was cool. Let's make a Breakout clone on our BadgerStick!

Hardware

Required Components

We will need a few other components to make a simple controller for the BadgerStick.

More Soldering

To begin, snap off 15 pins from the break-away headers, and solder them to the through-holes on the side opposite the LED array of the BadgerStick.

Solder pins to the BadgerStick

Solder the Thumb Joystick to the Thumb Joystick Breakout board.

Solder joystick to breakout board

Snap off 5 pins from the break-away headers, and solder them to the through-holes on the Joystick Breakout Board.

Solder pins to joystick breakout board

Connections

Place the BadgerStick in the breadboard with pin 10 in position i13 and pin 5V in position i27.

Connect the rest of the components as follows:

Component Breadboard
Thumb Joystick Breakout* i7 (VCC) i6 (VERT) i5 (HOR) i3 (GND)
Pushbutton c20 c22 f20 f22
Pushbutton c28 c30 f28 f30
Jumper Wire ( - ) g30
Jumper Wire ( - ) g25
Jumper Wire ( - ) g22
Jumper Wire ( - ) j3
Jumper Wire j7 g23
Jumper Wire j6 g18
Jumper Wire j5 g17
Jumper Wire g21 g28

* Pins not listed are not used.

Gaming badger

IMPORTANT: You can leave the battery pack soldered into the BadgerStick if you desire. If you remove the battery pack, you will need to supply power through another means, such as a USB port or a USB extension cable.

You should now have a makeshift game controller with a tiny LED screen!

Gaming badger with batteries

The Code

In a new Arduino sketch window, copy in the following code:

language:c
/****************************************************************
BadgerHack_Breakout.ino

This code is beerware; if you see me (or any other SparkFun 
employee) at the local, and you've found our code helpful, please
buy us a round!

Distributed as-is; no warranty is given.
****************************************************************/

#include <SparkFun_LED_8x7.h>
#include <Chaplex.h>

// Constants
#define DEBUG                1
#define FPS                  60
#define SENSITIVITY          100
#define MAX_X_SPAN           127
#define PADDLE_SIZE          2
#define INITIAL_BALL_SPEED   0.1
#define BALL_SPEED_INC       0.004
#define PAUSE_BEFORE_SHOOT   1000    // ms
#define ROW_SIZE             7
#define COL_SIZE             8
#define FIELD_SIZE           ROW_SIZE * COL_SIZE

// Pin definitions
#define RNG_SEED_PIN  2
#define X_PIN         0
#define Y_PIN         1
#define BUTTON_1_PIN  3
#define BUTTON_2_PIN  4

// Global variables
byte led_pins[] = {2, 3, 4, 5, 6, 7, 8, 9}; // Pins for LEDs
uint16_t horz_zero;
uint16_t vert_zero;
uint8_t paddle_size;

// Setup
void setup() {

#if DEBUG
  Serial.begin(9600);
  Serial.println(F("Breakout demo for BadgerHack"));
#endif

  // Initialize and clear display
  Plex.init(led_pins);
  Plex.clear();
  Plex.display();

  // Seed our random number generator
  randomSeed(analogRead(2));

  // Calibrate our joystick by finding the center
  horz_zero = analogRead(X_PIN);
  vert_zero = analogRead(Y_PIN);
}

// Loop - play the game forever
void loop() {

  // Play the game inifinity times
  playGame();
}

/****************************************************************
 * Functions
 ***************************************************************/

// Play the game
void playGame() {

  // Calculate the new x max based on paddle size
  paddle_size = PADDLE_SIZE;
  uint16_t field_max = MAX_X_SPAN - 
                        (paddle_size - 1) * (MAX_X_SPAN / 7);

  // Create new game variables
  boolean playing;
  boolean win;
  unsigned long frame_start;
  uint8_t millis_per_frame = 1000/FPS;
  unsigned long game_start;
  boolean ball_moving;
  int16_t paddle_move;
  int16_t paddle_field = field_max / 2;
  uint8_t paddle_x;
  float ball_x = 3;
  float ball_y = 5;
  float inc_x;
  float inc_y;
  float ball_speed;
  uint8_t ball_round_x;
  uint8_t ball_round_y;  
  uint16_t ball_theta;
  boolean can_deflect = true;
  int i;
  uint8_t x;
  uint8_t y;
  byte the_wall[] = { 1,1,1,1,1,1,1,
                      1,1,1,1,1,1,1,
                      1,1,1,1,1,1,1,
                      1,1,1,1,1,1,1,
                      0,0,0,0,0,0,0,
                      0,0,0,0,0,0,0,
                      0,0,0,0,0,0,0,
                      0,0,0,0,0,0,0 };
#if DEBUG
  Serial.println("New game!");
  Serial.print("Field span: ");
  Serial.println(field_max);
#endif

  // Note when we start the game (so we can shoot the ball)
  game_start = millis();
  ball_moving = false;

  // Assign an initial direction and speed to the ball
  ball_theta = initBallTheta();
  ball_speed = INITIAL_BALL_SPEED;

  // Play the game until we win or lose
  playing = true;
  while ( playing ) {

    // For each frame, aim for refresh rate
    frame_start = millis();

    // Check for a win condition
    win = true;
    for ( i = 0; i < FIELD_SIZE; i++ ) {
      if ( the_wall[i] > 0 ) {
        win = false;
        break;
      }
    }
    if ( win ) {
      Plex.clear();
      Plex.scrollText("You win!", 1);
      delay(5000);
      Plex.stopScrolling();
      playing = false;
    }

    // Read the value of the joystick and map to a movement
    paddle_move = analogRead(X_PIN) - horz_zero;
    paddle_move = paddle_move / SENSITIVITY;
#if 0
    Serial.print("Moving: ");
    Serial.println(paddle_move);
#endif

    // Move the paddle and calculate its real x position
    paddle_field = paddle_field + paddle_move;
    if ( paddle_field <= 0 ) {
      paddle_field = 0;
    }
    if ( paddle_field >= field_max ) {
      paddle_field = field_max;
    }
    paddle_x = map(paddle_field, 0, field_max,
                   0, 6 - (paddle_size - 1));

    // If the ball has been shot, move it
    if ( ball_moving ) {

      // Calculate the ball's new position
      ball_x += ball_speed * cos(ball_theta * (M_PI / 180));
      ball_y += ball_speed * sin(ball_theta * (M_PI / 180));

      // Check the ball against the paddle
      if ( (ball_y > 6) &&
            (ball_x >= paddle_x) &&
            (ball_x <= (paddle_x + (paddle_size - 1))) &&
            can_deflect ) {
        ball_y = 6 - abs(6 - ball_y);
        ball_theta = 360 - ball_theta;
        can_deflect = false;
      }

      // Allow ball to be deflected once it leaves paddle range
      if ( ball_y <= 6 ) {
        can_deflect = true;
      }

      // Check if the ball moved past the paddle (lose)
      if ( ball_y > 7 ) {
#if DEBUG
        Serial.print("LOSE! x=");
        Serial.print(ball_x);
        Serial.print(" y=");
        Serial.print(ball_y);
        Serial.print(" Paddle:");
        Serial.print(paddle_x);
        Serial.print("-");
        Serial.println(paddle_x + paddle_size - 1);
#endif
        playing = false;
      }

      // Check the ball against the walls (and bounce!)
      if ( ball_y < 0 ) {
        ball_y = abs(ball_y);
        ball_theta = 360 - ball_theta;
      }
      if ( ball_x < 0 ) {
        ball_x = abs(ball_x);
        ball_theta = (540 - ball_theta) % 360;
      }
      if ( ball_x > 6 ) {
        ball_x = 6 - abs(6 - ball_x);
        ball_theta = (540 - ball_theta) % 360;
      }

      // Bounce if we hit a block above the ball
      i = (floor(ball_y) * ROW_SIZE) + roundFloat(ball_x);
      if ( the_wall[i] > 0 ) {
        the_wall[i]--;
        ball_y = (i / ROW_SIZE) + abs((i / ROW_SIZE) - ball_y);
        ball_theta = 360 - ball_theta;
        ball_speed += BALL_SPEED_INC;
      }

      // Bounce if we hit a block below the ball
      i = (ceil(ball_y) * ROW_SIZE) + roundFloat(ball_x);
      if ( the_wall[i] > 0 ) {
        the_wall[i]--;
        ball_y = (i / ROW_SIZE) - abs((i / ROW_SIZE) - ball_y);
        ball_theta = 360 - ball_theta;
        ball_speed += BALL_SPEED_INC;
      }

      // Bounce if we hit a block to the left the ball
      i = (roundFloat(ball_y) * ROW_SIZE) + floor(ball_x);
      if ( the_wall[i] > 0 ) {
        the_wall[i]--;
        ball_y = (i / ROW_SIZE) + abs((i / ROW_SIZE) - ball_y);
        ball_theta = (540 - ball_theta) % 360;
        ball_speed += BALL_SPEED_INC;
      }

      // Bounce if we hit a block to the right the ball
      i = (roundFloat(ball_y) * ROW_SIZE) + ceil(ball_x);
      if ( the_wall[i] > 0 ) {
        the_wall[i]--;
        ball_y = (i / ROW_SIZE) - abs((i / ROW_SIZE) - ball_y);
        ball_theta = (540 - ball_theta) % 360;
        ball_speed += BALL_SPEED_INC;
      }

    } else {

      // See if we need to start moving the ball
      if ( millis() >= game_start + PAUSE_BEFORE_SHOOT ) {
        ball_moving = true;
      }
    }

    // Round the ball's position to the nearest pixel
    ball_round_x = roundFloat(ball_x);
    ball_round_y = roundFloat(ball_y);

    // Draw tbe wall, the paddle, and the ball
    Plex.clear();


    for ( y = 0; y < COL_SIZE; y++ ) {
      for ( x = 0; x < ROW_SIZE; x++ ) {
        if ( the_wall[(x * ROW_SIZE) + (ROW_SIZE - 1 - y)] > 0 ) {
          Plex.pixel(x, y);
        }
      }
    }
    for ( i = 0; i < paddle_size; i++ ) {
      Plex.pixel(7, map(paddle_x + i, 0, 6, 6, 0));
    }
    Plex.pixel(ball_round_y, map(ball_round_x, 0, 6, 6, 0));
    Plex.display();

    // Wait until we reach our target end of frame
    while ( millis() < frame_start + millis_per_frame ) {
      delay(1);
    }
 #if 0
   Serial.print("FPS: ");
   Serial.println( 1000 / (millis() - frame_start) );
 #endif

  }
}

// Create a randomized ball launch angle
unsigned int initBallTheta() {

  unsigned int theta;

  // Choose an angle  in the range of 210-239 deg or 301-330 deg
  theta = random(0, 60);
#if DEBUG
  Serial.print("RNG:");
  Serial.print(theta);
#endif
  if ( theta < 30 ) {
    theta = 210 + theta;
  } else {
    theta = 271 + theta;
  }

#if DEBUG
  Serial.print(" Theta:");
  Serial.println(theta);
#endif

  return theta;
}

// Rounds a floating value to an integer
int roundFloat(float x) {
  if ( x >= 0 ) {
    return (int) (x + 0.5);
  }
  return (int) (x - 0.5);
}

Play

Upload the program to the BadgerStick, and prepare to play!

Use the joystick to move the paddle back and forth to bounce the ball. You win when you "break" all the lights on the top part of the screen. You lose if you let the ball go past your paddle.

Let's play Breakout!

You might notice that we do not use the 2 buttons in the game. Breakout only requires a joystick. However, you now have a basic platform that is perfect for creating games!

What other games would you want to make? Here are some ideas: