Powering LilyPad LED Projects

≡ Pages
Contributors: Gella , MikeGrusin

Conductive Thread Resistance

One of the most important things to consider when building a wearable project is the resistance of conductive thread. Unlike copper wire, which has very little resistance, conductive thread's resistance will vary depending on the metal used to make the thread and the thickness of the thread. Most conductive threads list resistance in Ohms/Ft. The lower this number is, the better, because less resistance means more electricity can get through to the components used in your project.

alt text

The basic electrical property Ohm’s Law states that running an electrical current through a material high in resistance causes the voltage to drop. The higher the current, the greater the voltage drop. This means that even though a LiPo battery powering your LilyPad may put out 3.7 volts, by the time it gets through the thread to your components, it may drop to 3.0 volts or less.

Many electrical components, such as LEDs, need a certain voltage to function properly. For example, in a project with LilyPad LEDs if the voltage drops below 3 volts, a blue LED will stop working, followed by the green and finally the red. To get full-color output from RGB LEDs like the LilyPad RGB LED Board, you should always try to run at 3 volts or above.

Forward voltages of LilyPad LEDs

LilyPad LEDForward Voltage
Blue3.2 Volts
Green3.2 Volts
Pink2.5 Volts
Purple (retired)2.8 Volts
Red2.0 Volts
White3.3 Volts
Yellow2.0 Volts

Forward voltages of LilyPad RGB LEDs:

LilyPad LEDRed LED Forward VoltageGreen LED Forward VoltageBlue LED Forward Voltage
LilyPad Tri-Color LED2.0 Volts3.5 Volts3.5 Volts
LilyPad Pixel Board2.2 Volts3.4 Volts3.4 Volts

To minimize voltage drop, we'll need to decrease the resistance of the power connections. There are a few ways to do this:

  • Keep the length of the power connections as short as possible. Because the resistance increases with length, if you reduce the length, you’ll reduce the resistance.

  • Reduce the resistance of the thread itself. Thicker thread has a lower resistance than thinner thread, and using multiple strands at a time reduces the resistance even further.

TIP:
Use a non conductive thread to stitch bundled thread (either placed together or braided) to your base fabric. Leave enough open spaces in the stitching so you are able to stitch conductive thread to the larger thread bundle when connecting components. This video from e-textile expert Lynne Bruning shows this technique at around the 4:10 mark:

Conductive Thread Alternatives:

For large projects that require thread to travel long distances, projects with a lot of power-hungry pieces such as a large amount of LilyPad Pixel Boards, or in spots where thread may break under stress, here are some alternatives that work well for wearables:

Conductive Ribbon

Conductive Ribbon - 3-Conductor (1 yard)

DEV-10172
Retired

Specialty nylon ribbon with flexible stranded wire woven into it is a great alternative to conductive thread with low resistance. You will need to solder to the tinsel within the ribbon in order to use in a project.

Conductive Fabric Traces

Conductive Fabric - 12"x13" Ripstop

DEV-10056
Retired

Conductive Fabric - 12"x13" MedTex130

DEV-10070
Retired

You can create your own low resistance traces using thin strips of conductive fabric. We recommend using iron-on adhesive to attach to fabric or ribbon, then using conductive thread to hand stitch components to the traces.

alt text

Don't forget to insulate the fabric traces as you would conductive thread.

Stranded Wire

Ribbon Cable - 6 wire (15ft)

CAB-10646
$4.50

Another alternative is to switch from conductive thread to traditional wire. Wire has a much lower resistance than thread, allowing you to use more LEDs than a conductive thread circuit. You’ll have to switch from sewing to soldering, but it’s easy to solder wires to the same sew tabs to which you would normally connect thread.

Wire is prone to breaking if it is flexed repeatedly. For wearable projects that require maximum flexibility, use stranded wire (not solid), and look for special silicone-jacketed wire that is extremely flexible. For projects that will be washed, water may wick into exposed stranded wire, becoming trapped and potentially corroding it over time. Apply a small dab of silicone sealant to the cut ends of the wire to prevent this from happening.

If you have never soldered before or worked with wire, we recommend visiting the following tutorials.

How to Solder: Through-Hole Soldering

This tutorial covers everything you need to know about through-hole soldering.

Working with Wire

How to strip, crimp, and work with wire.