Crypto Shield Hookup Guide

This Tutorial is Retired!

This tutorial covers concepts or technologies that are no longer current. It's still here for you to read and enjoy, but may not be as useful as our newest tutorials.

≡ Pages
Contributors: jbdatko, CaseyTheRobot

Using the CryptoShield

There are two ways to use this shield:

  1. With Linux on a board like the following. Not all of these have been tested, this is just a list of boards that claim to support Linux and support the physical Arduino form factor:


    1. Any board that directly supports the Arduino IDE and the Arduino form-factor.

IO Voltage Levels

The CryptoShield is 3.3V and 5V friendly. The CryptoShield contains onboard logic level conversion circuitry. If the main board is properly supplying IOREF, as per the Arduino board specification, then the CryptoShield should work without any external voltage conversion.