Spectacle Light Board Hookup Guide

≡ Pages
Contributors: SFUptownMaker

Example Project

Let's use the Spectacle Light Board to put together a working project! We're going to use a "virtual board" to blink a lightstrip attached to the Light Board.

Connect the boards

To follow along with this tutorial, you'll need the following hardware:

Wall Adapter Power Supply - 5.1V DC 2.5A (USB Micro-B)

TOL-13831
$13.95

LED RGB Strip - Addressable, Bare (1m)

COM-12025
Retired

Spectacle Director Board

DEV-13912
Retired

Spectacle Light Board

DEV-14052
Retired

JST to JST-SM Wire - 1ft

CAB-14165
Retired

Note that you will need two of the TRRS cables!

First, plug one end of one of the TRRS cables into the "Direct" jack on the Director Board.

The direct jack

Next, take the other TRRS cable and plug it into the "Program" jack on the Director Board.

The program jack

Take the other end of this cable and plug it into the audio jack of the phone, tablet, or computer that you'll be using to program the system.

Into the phone jack

Now, plug the free end of the first cable into the "In" jack on the Light Board. Pay attention to which jack you plug into, as the two jacks are directional.

Light board input jack

Next, you'll need the JST-SM to JST-PH adapter cable. Plug the white end into connector position 0 on the Light Board.

Adapter into light board

Plug the black end of the adapter into the mating connector on the light strip.

Adapter into light strip

Finally, plug the Micro B end of the power adapter into the Director Board, and the other end into the wall. You should see one solid light and one blinking light on the Light Board. On the Director Board, you'll see one solid light and one light which blinks one time, then pauses, then repeats. This shows that power is present and the boards are up and running.

Setting up the board configuration

Blank project page

When you first open the Spectacle app webpage, this is what you'll see. Your project name will differ from mine, as Spectacle assigns a random name to each project.

add a board button

To continue, we must tell the project which boards we wish to use. Start by clicking the "Add a board" button at the bottom of the page.

List of available boards

This will bring up a list of the available boards. Click anywhere in the "Lights" box to add a Light Board to the system.

Light board edit button

Now that you've added the Light Board, it's time to add the actions to the light board. To get a blink effect, we're going to trigger two events on one signal, and make one delayed slightly. Click the clapboard icon as highlighted in the above picture to bring up the list of actions assigned to that board.

No actions assigned

Naturally, there are no actions in the list, since we haven't added any yet. Click the "Add an Action" button at the bottom of the screen to bring up a list of available actions.

Actions list for light board

Here's the list of Light Board actions that will pop up when you hit the "Add an Action" button. We want to add an action of the "Fill Color" type, so click on that entry.

alt text

Here's the "Fill Color" action list of options. See the previous page of the tutorial for information about the various fields.

Fill with settings in place

Fill in the blanks of the page as seen above. This sets up the strip to turn on to solid white when an event hits channel 0. Now, add another "Fill Color" type action and scroll down so it's completely visible.

settings for second fill page

Once you've added the second "Fill Color" action, set the fields as shown above. This will cause it to trigger on the same action as the first fill, but it won't activate for two seconds. Then, it will set all the lights on the strip to "black" (off).

Go back button

Click the "Go Back" button to return to the main screen. Clicking this button automatically saves your work, as well.

Now, repeat the steps from above to add a Virtual Board. Click the clapboard icon to edit the list of actions for the Virtual Board.

Virtual Boards provide a number of functions outside of the normal operation of Spectacle boards. In this case, we want "Periodic Input", which generates a signal at a fixed timing rate.

list of Virtual Board actions

Here are the actions we can use with a Virtual Board. We want a "Periodic Input", to create our blinking action.

Periodic settings

You should set up the periodic action to match the settings above. This will generate a short pulse every 10 seconds. Now click "Go Back" again to return to the main page.

Finished project

Congratulations! You've finished the configuration step of the process. Now it's time to move on to loading the project onto your Director Board.

Uploading

Now that you've created your Spectacle program it's time to upload it to the Director Board. If you followed the instructions above, your uploading device is connected to the board and ready to go, so all you need to do is touch the "Install Script" button at the bottom of the page. That will bring up the page seen below.

Upload page

Make sure the volume on your device is turned all the way up, and that no other audio source (music, video, etc) is playing in the background. Then press and hold the "RST" button on the Director Board, press and hold the "PROG" button, then release the "RST" button.

This will put the Director Board into program mode. You'll see the light on the board blink three times, pause, then repeat. This is your visual indicator that the board is in program mode. Once you've established that the board is in program mode, you can begin programming by touching the "Install" button on the Spectacle app screen. The button will gray out during the programming process, which should only last for a few seconds. Once programming is done, you'll see the light on the Director Board blink 10 times, pause, then repeat. That's your cue that the program was uploaded successfully.

Press the "RST" button again to reset the system and begin the program!

If you have any troubles, visit the troubleshooting page for help resolving your issues.