LDK Experiment 5: Make Your Own Switch a learn.sparkfun.com tutorial

Available online at: https://sfe.io/t45

Contents

Introduction

Welcome to experiment 5 of the LilyPad Design Kit, where you’ll learn to create your own easy, inexpensive switch using textile components!

Suggested Reading

Before we begin, here are a few resources you might find helpful:

Previous LDK Tutorials

Other Relevant Tutorials

Gather Materials

These are the parts you’ll need to construct this circuit. If you’re using the LilyPad Design Kit, you’ve already got them all.

alt text

You’ll also want to have felt (included in the kit), scissors, fabric, an embroidery hoop, and possibly a needle threader.

Go ahead and get your fabric prepped on the embroidery hoop and your needle threaded.

fabric in hoop

Positive trace

In making a switch, we’re trying to create a connection that we can engage that will stay engaged until we disengage it. Much like a light switch, we will turn it on, and it will stay on until we turn it off.

cut felt

Start by cutting a small strip off of your felt, about half an inch wide and 2-3 inches long.

positive battery to felt

Place your battery holder where you’d like it, and stitch the positive pins to the fabric and each other with conductive thread. Continue the trace another inch or so in the direction you’d like your LED to go. Lay down the strip of felt you cut with one thin end next to your trace and the other thin end pointing towards your planned LED location. Sew a few stitches around the close edge of the felt, attaching it firmly to the fabric.

stitched through felt

Continue the trace up the length of the felt, no longer stitching through the fabric. This should result in a strip of felt attached at one end to the fabric, free along the rest of its length, with a trace of conductive thread all the way up.

snap on felt

At the detached edge, where your trace stops, stitch the male (the one with the bump sticking out) side of the snap to the bottom of the felt strip. The bump should point towards the fabric. There are small holes around the edge of the snap to allow it to be sewn down. When it’s firmly attached, knot and cut the thread.

snap on fabric

Beginning a new trace, sew the female side of the snap, with the hole facing up, to the fabric below the male side. This should allow the two snaps to mate when the felt strip is at full extension.

snap to positive LED

Stitch from the snap to where you’d like the positive pin of the LED to be, and sew the LED down. Knot and cut your thread.

Negative trace

negative LED pin

Beginning with a new thread, sew down the negative pin of the LED.

negative LED to battery

From here, sew a trace back to the negative pins of the battery pack and stitch those down as well.

snapped and lit!

That’s it! Slide your battery into the battery holder, positive side up, and turn on the switch on the battery pack. Try snapping and unsnapping your felt switch a few times. When it’s snapped, the light will turn on, unsnapped, it will turn off!

Resources and Going Further

Want more? Check out LDK Experiment 6 for more e-textile fun.

Want to try some more complex e-textiles projects, or experiment with other e-textile switches? Check out these other great tutorials.

Or check out this blog post.

Hardware Hump Day: 3 Soft Electronics Tricks

December 28, 2016

Read Post

6 Easy DIY Soft Components

March 7, 2018

Read Post


learn.sparkfun.com | CC BY-SA 3.0 | SparkFun Electronics | Niwot, Colorado