Arduino, Processing and Max
SparkFun's Department of Education taught a workshop at the Boulder Museum of Contemporary Arts alongside Darwin Grosse, the Director of Engineering for Cycling '74. We gave artists and introduction to not only Arduino but also Processing in three and a half hours which they then connected to Max using the patch posted here. These materials are intended for use with SparkFun's Danger Shield but can easily be adapted for use with any Arduino and sensor combination.
Materials by Linz Craig, Ben Leduc-Mills and Dave Stillman
Max Patch by Darwin Grosse
Note You may need to delete and re-enter the serial code in order to make the patch work. Then use the r command to receive the sensor values and use in Max.
Downloads
DangerConnect.maxpat.zip
MediaLive.ino.zip
MediaLive_DangerShield_Processing.ppt
mediaLive_Processing02.zip
- Author: Lindsay Craig
- Date Posted: February 6, 2014
- Tags
- License
- resources are open sourced under CC BY-SA 3.0