SparkFun ProDriver Hookup Guide
Contributors:
QCPete, Santa Claus Impersonator
Resources and Going Further
For more on the SparkFun ProDriver (TC78H670FTG), check out the links below:
- Schematic (PDF)
- Board Dimensions (PDF)
- Eagle Files (ZIP)
- TC78H670FTG Datasheet (PDF)
- Arduino Library
- GitHub Repository
- Product Showcase
For more motor control tutorial, check out the links below:
GPS Differential Vector Pointer
Use GPS to have two objects, a base and a target, point towards one another. This can be used to aim a directional antenna (or in the case of this project, a laser) from one object to the other object at a distance that is only limited by your ability to provide the base station with the target's GPS location.
Blynk Board Project Guide
A series of Blynk projects you can set up on the Blynk Board without ever re-programming it.
Clap On Lamp
Modify a simple desk lamp to respond to a double clap (or other sharp noise) using parts from the SparkFun Inventor's Kit v4.0.
WiFi Controlled Robot
This tutorial will show you how to make a robot that streams a webcam to a custom website that can be remotely controlled.
Getting Started with the Autonomous Kit for the Sphero RVR
Want to get started in robotics? Look no further than the SparkFun autonomous kit for the Sphero RVR! Whether you purchased the Basic or Advanced kit, this tutorial will get you rolling...
Or check out this blog post for inspiration