Installing Arduino IDE

Pages
Contributors: bboyho, b_e_n
Favorited Favorite 17

Introduction

This tutorial will walk you through downloading, installing, and testing the Arduino software (also known as the Arduino IDE - short for Integrated Development Environment). Before you jump to the page for your operating system, make sure you've got all the right equipment.

Arduino Logo

Required Materials

To follow along with this tutorial, you will need the following materials. You may not need everything though depending on what you have. Add it to your cart, read through the guide, and adjust the cart as necessary.

  • A computer (Windows, Mac, or Linux)
  • An Arduino-compatible microcontroller (anything from this guide should work)
  • A USB A-to-B cable, or another appropriate way to connect your Arduino-compatible microcontroller to your computer (check out this USB buying guide if you're not sure which cable to get).
Arduino Uno - R3

Arduino Uno - R3

DEV-11021
$27.60
138
USB Cable A to B - 6 Foot

USB Cable A to B - 6 Foot

CAB-00512
$4.50
1

Suggested Reading

If you're new to Arduino in general, you'll want to check out this tutorial to familiarize yourself with everyone's favorite microcontroller platform.

What is an Arduino?

February 26, 2013

What is this 'Arduino' thing anyway? This tutorials dives into what an Arduino is and along with Arduino projects and widgets.

If you're ready to get started, click on the link in the column on the left that matches up with your operating system, or you can jump to your operating system here.

Downloading the Arduino IDE

You can download the Arduino IDE from their website. They have installation instructions, but we will also go over the installation process as well. Make sure you download the version that matches your operating system.

The installation procedure is fairly straightforward, but it does vary by OS. Here are some tips to help you along.

Troubleshooting Tips
  • We recommend using a computer with a full desktop operating system like Windows 7/10 (avoid Windows 8 if you can), Mac OSX, and certain flavors Linux (check the Arduino FAQ page for compatibility).

    • If you are not a technical or computer savy individual and you have your choice of computers, I highly recommend using a Windows 7, 10, or 11 computer. You will usually run into the the least issues, if any, with these operating systems.

  • We do NOT recommend using a Chromebook, Netbook, tablet, phone, or the Arduino Web IDE in general. You will be responsible for troubleshooting any driver or Arduino Web IDE issues.

  • As of the writing of this tutorial (updated 12-14-2018), the most recent and stable release of the Arduino IDE is version 1.8.5. We recommend using that version of the Arduino IDE; you can download the previous releases here.

  • Raspberry Pi users with Raspbian installed should use the Linux ARM download. We do not recommend using the command line installation. It will install the oldest release of Arduino, which is useless when it comes to installing new boards definitions or libraries.

  • For additional troubleshooting tips, here is a troubleshooting guide from Arduino.

Windows

This page will show you how to install and test the Arduino software with a Windows operating system (Windows 10, Windows 7, Vista, and XP).

Go to the Arduino download page and download the latest version of the Arduino software for Windows if you have not already.

Installer

The Windows version of Arduino is offered in two options: an installer or a zip file. The installer is the easier of the two options, just download that, and run the executable file to begin the installation.

Windows 10 - Arduino Installation Diagram

Windows install steps. Click the image to get a bigger view.

When you're prompted to install a driver during installation, select "Install". This will install drivers for Arduino specific boards (like the Uno, Nano, etc.) that you may use in the future.

ZIP

If you choose to download the zip file version of Arduino, you'll need to extract the files yourself. Don't forget which folder you extract the files into! You will need to run the executable Arduino file in the folder to start the Arduino IDE.

When the download is finished, un-zip it and open up the Arduino folder to confirm that yes, there are indeed some files and sub-folders inside. The file structure is important so don't be moving any files around unless you really know what you're doing.

Connecting Your Arduino

Power up your Arduino by connecting your Arduino board to your computer with a USB cable (or FTDI cable if you're using an Arduino Pro). You should see the an LED labeled 'ON' light up. (this diagram shows the placement of the power LED on the UNO).

Drivers for Arduino Uno on Windows

To install the drivers for the Arduino Uno, you will need to plug in your board to your computer's USB port. Once the board is connected, you will need to wait for Windows to begin it's driver installation process. After a few moments, the process will probably fail, despite its best efforts.

Open up a search, type in Device Manager, and hit ENTER.

Search for Device Manager

Look under Ports (COM & LPT) tree. You should see an open port named "Arduino UNO (COMxx)". If there is no COM & LPT section, look under "Other devices" for "Unknown Device. Right click on the "Arduino UNO (COMxx)" or "Unknown device" port and choose the "Update Driver Software" option.

alt text

Next, choose the "Browse my computer for Driver software" option

alt text

Finally, navigate to the Arduino IDE folder. This should be where you unzipped the Arduino IDE (e.g. it should be similar to the following path with a different version number: C:\Program Files\arduino-1.8.5\drivers). Depending on what version of Windows you have, you may be able to select the Uno's driver file, named "Arduino.inf", located in the "Drivers" folder (not the "FTDI USB Drivers" sub-directory). If you cannot see the *.inf file, it is probably just hidden. You can select the "drivers" folder with the "include sub-folders" option selected instead.

alt text

Windows will finish up the driver installation from there! Your computer will enumerate with a COM port. You may see a COM port number depending on what is currently saved in your computer. Try to remember what the number is when uploading. If not, you can always navigate back to the device manager and power cycle the Arduino to determine what number your Arduino enumerated on.

alt text

For earlier versions of the Arduino boards (e.g. Arduino Duemilanove, Nano, or Diecimila) check out this page for specific directions.

Drivers for RedBoard on Windows

Depending on your board, there may be different USB-to-serial converters on your board. If you are using a RedBoard you will need to go to the How to Install FTDI Drivers tutorial. If you are using the or RedBoard Qwiic, you will need to go to the How to Install CH340 Drivers tutorial. Make sure to look closely at your board and its respective hookup guide to determine USB-to-serial converter that is on board.

How to Install FTDI Drivers

June 4, 2013

How to install drivers for the FTDI Basic on Windows, Mac OS X, and Linux.

How to Install CH340 Drivers

August 6, 2019

How to install CH340 drivers (if you need them) on Windows, Mac OS X, and Linux.

Launch and Blink!

After following the appropriate steps for your software install, we are now ready to test your first program with your Arduino board! Launch the Arduino application. If you disconnected your board, plug it back in.

alt text

Open the Blink example sketch by going to: File > Examples > 01.Basics > Blink.

alt text

Select the type of Arduino board you're using: Tools > Board > Arduino Uno.

alt text

Select the serial/COM port that your Arduino is attached to: Tools > Port > COMxx. In this case it was COM11.

alt text

With your Arduino board connected, and the Blink sketch open, press the "Upload" button.

alt text

After a second, you should see some LEDs flashing on your Arduino, followed by the message "Done Uploading" in the status bar of the Blink sketch.

alt text

If everything worked, the onboard LED on your Arduino should now be blinking! You just programmed your first Arduino!

Troubleshooting

This guide from Arduino has some more details and troubleshooting tips if you get stuck.

Mac

This page will show you how to install and test the Arduino software on a Mac computer running OSX.

Go to the Arduino download page and download the latest version of the Arduino software for Windows if you have not already.

When the download is finished your Mac should automatically un-zip the contents. This will probably in your Downloads folder.

alt text

You can leave the program in the Downloads folder or move it into your Applications folder.

alt text

Connecting Your Arduino

Power up your Arduino by connecting your Arduino board to your computer with a USB cable (or FTDI cable if you're using an Arduino Pro). You should see the an LED labeled 'ON' light up. (this diagram shows the placement of the power LED on the UNO).

Drivers for Arduino Uno on Mac

For the Arduino Uno, you do not need to install drivers for Mac! You can skip on down and try uploading a blink sketch!

Drivers for RedBoard on Mac

Depending on your board, there may be different USB-to-serial converters on your board. If you are using a RedBoard you will need to go to the How to Install FTDI Drivers tutorial. If you are using the or RedBoard Qwiic, you will need to go to the How to Install CH340 Drivers tutorial. Make sure to look closely at your board and its respective hookup guide to determine USB-to-serial converter that is on board.

How to Install FTDI Drivers

June 4, 2013

How to install drivers for the FTDI Basic on Windows, Mac OS X, and Linux.

How to Install CH340 Drivers

August 6, 2019

How to install CH340 drivers (if you need them) on Windows, Mac OS X, and Linux.

Launch and Blink!

After following the appropriate steps for your software install, we are now ready to test your first program with your Arduino board!

Launch the Arduino application wherever the program is located. If you disconnected your board, plug it back in.

alt text

Open the Blink example sketch by going to: File > Examples > 01.Basics > Blink.

alt text

Select the type of Arduino board you're using: Tools > Board > Arduino Uno.

alt text

Select the serial port that your Arduino is attached to: Tools > Port > xxxxxx. It'll probably look something like "/dev/tty.usbmodemfd131" or "/dev/tty.usbserial-131" but probably with a different number. In this case, it was /dev/cu.usbmodemFD131.

alt text

With your Arduino board connected and the Blink sketch open, press the "Upload" button.

alt text

After a second, you should see some LEDs flashing on your Arduino, followed by the message "Done Uploading" in the status bar of the Blink sketch.

alt text

If everything worked, the onboard LED on your Arduino should now be blinking! You just programmed your first Arduino!

Troubleshooting

If you're having problems, check out this troubleshooting guide from Arduino.

Linux

If you are a Linux user, you probably know that there are many different distribution 'flavors' of Linux out there. Unsurprisingly, installing Arduino is slightly different for many of these distributions. Luckily, the Arduino community has done an excellent job of providing instructions for most of the popular versions. Click on the link below that covers your flavor of Linux:

If the above directions did not work for you, or you don't see your distribution, try this catch-all guide.

You can go to the download page and download the latest version of Arduino for Linux (there are 32-bit and 64-bit versions available) when your system is properly set up.

Connecting Your Arduino

Power up your Arduino by connecting your Arduino board to your computer with a USB cable (or FTDI cable if you're using an Arduino Pro). You should see the an LED labeled 'ON' light up. (this diagram shows the placement of the power LED on the UNO).

ZIP

Once you download the zip file version of Arduino, you'll need to extract the files yourself. Don't forget which folder you extract the files into! Once downloaded, open a serial terminal and navigate to the Arduino program folder that was unzipped using the cd command and the folder path. In this case, we downloaded Arduino IDE v1.8.5, 64-bit version for the Ubuntu distribution. The path and folders may be different depending on the version that is downloaded. You may need to use the ls command to navigate.

language:bash
cd /Downloads/arduino-1.8.5-linux64/arduino-1.8.5

Once you are in the Arduino program folder, you'll need to enter the following command in the terminal window to install.

language:bash
./install.sh

At this point, your terminal window will probably look like the following.

alt text

When finished, the Arduino IDE will be installed on the desktop!

Drivers for RedBoard on Linux

For the Arduino Uno, you do not need to install drivers for Linux! You may need to change the COM port permissions which will be explained further below. You can skip on down and try uploading a blink sketch!

Drivers for RedBoard on Linux

Depending on your board, there may be different USB-to-serial converters on your board. If you are using a RedBoard you will need to go to the How to Install FTDI Drivers tutorial. If you are using the or RedBoard Qwiic, you will need to go to the How to Install CH340 Drivers tutorial. Make sure to look closely at your board and its respective hookup guide to determine USB-to-serial converter that is on board.

How to Install FTDI Drivers

June 4, 2013

How to install drivers for the FTDI Basic on Windows, Mac OS X, and Linux.

How to Install CH340 Drivers

August 6, 2019

How to install CH340 drivers (if you need them) on Windows, Mac OS X, and Linux.

Launch and Blink!

After following the appropriate steps for your software install, we are now ready to test your first program with your Arduino board!

Launch the Arduino application. If you disconnected your board, plug it back in.

Open the Blink example sketch by going to: File > Examples > 01.Basics > Blink.

alt text

Select the type of Arduino board you're using: Tools > Board > Arduino Uno.

alt text

Select the serial port that your Arduino is attached to: Tools > Port > xxxxxx (it'll probably look something like "/dev/ttyACM0" but probably with a different number)

alt text

With your Arduino board connected and the Blink sketch open, press the "Upload" button.

alt text

After a second, you should see some LEDs flashing on your Arduino, followed by the message "Done Uploading" in the status bar of the Blink sketch.

alt text

If everything worked, the onboard LED on your Arduino should now be blinking! You just programmed your first Arduino!

Troubleshooting

The Arduino Playground Linux section is a great resource for figuring out any problems with your Arduino installation.

Board Add-Ons with Arduino Board Manager

With Arduino v1.6.4+, a new boards manager feature makes it easy to add third-party boards (like the SparkFun RedBoard, Digital Sandbox, and RedBot) to the Arduino IDE.

To start, highlight and copy (CTRL + C / CMD + C) the text below for the boards manager URL. You'll need this to configure Arduino.

language:bash
https://raw.githubusercontent.com/sparkfun/Arduino_Boards/main/IDE_Board_Manager/package_sparkfun_index.json

Additional Boards Manager URLs

Heads Up: GitHub has recently moved away from having default branches as "master" and changed the default to "main". SparkFun has followed this move as well. If you're unable to see a particular board inside of Arduino it may be that you are using the older "master" link. As a result, you will only see the previous changes on the old master branch. Please change to the 'main' json url listed above and all should be well.

Open up Arduino:

  • Configure the Boards Manager
    • For Windows and Linux, head to File > Preferences > Additional Boards Manager URLs and paste (CTRL + V / CMD + V) the link
    • For Macs, head to Arduino > Preferences > Additional Boards Manager URLs and paste (CTRL + V / CMD + V) the link
  • Click on Tools > Board > Boards Manager...
  • Select the Type as "Contributed" from the drop down menu.
  • Click on the SparkFun AVR Boards and then click Install.

That's it! Boards are all installed. This also gives you access to all of our library files as well through the built-in Library Manager tool in Arduino. Looking for more information about adding other custom boards? Check out the the following tutorial to install other Arduino cores.

Installing Board Definitions in the Arduino IDE

September 9, 2020

How do I install a custom Arduino board/core? It's easy! This tutorial will go over how to install an Arduino board definition using the Arduino Board Manager. We will also go over manually installing third-party cores, such as the board definitions required for many of the SparkFun development boards.

Resources and Going Further

Now that you've got the Arduino software installed on your system and tested it with your Arduino board successfully, you're ready for your next steps into the world of embedded electronics. If you want to learn about some of the concepts that will help you build your projects, check out some of the following tutorials:

Installing an Arduino Library

How do I install a custom Arduino library? It's easy! This tutorial will go over how to install an Arduino library using the Arduino Library Manager. For libraries not linked with the Arduino IDE, we will also go over manually installing an Arduino library.

How to Power a Project

A tutorial to help figure out the power requirements of your project.

Choosing an Arduino for Your Project

Examining the diverse world of Arduino boards and understanding the differences between them before choosing one for a project.


Or check out the some of the Adventures in Science videos focused on Arduino.

Looking for the right Arduino?

Check out our Arduino Comparison Guide! We've compiled every Arduino development board we carry, so you can quickly compare them to find the perfect one for your needs.

Take me there!

If you'd rather jump right in to building something, check out these links to projects here on learn as well as some other places to find Arduino-based projects:

Or any of our tutorials tagged with Arduino.

Transparent Graphical OLED Breakout Hookup Guide

The future is here! Our Qwiic Transparent Graphical OLED Breakout allows you to display custom images on a transparent screen using either I2C or SPI connections.

SparkFun Photodetector (MAX30101) Hookup Guide

The SparkFun Photodetector - MAX30101 (Qwiic) is the successor to the MAX30105 particle sensor, a highly sensitive optical sensor. This tutorial will get you started on retrieving the raw data from the MAX30101 sensor.

MicroMod STM32WB5MMG Hookup Guide

Add a powerful combination of computing power and wireless communication to your next MicroMod project with the SparkFun MicroMod STM32WB5MMG Processor.